Other Parts Discussed in Thread: OMAP3530
hi...
we r using omap3530 under wince6.0...
we have successfully configured the display drivers for the resolution 800*600...... we have configured it to this particular resolution since we want to use TV-out and TV-out supports a max resolution of 800*600.and we also succeeded in getting the TV-out work :)
we also succeeded in displaying on both LCD display and TV-out simultaneously.. :) but the problem now is we r having a LCD display of size 1024*600....
since our build resolution is 800*600 ,we get our LCD filled only 75% of its size(1024*600)....so we want our LCD screen to be filled completely...
so how can we SCALE the 800*600 resolution to 1024*600 so that it fits our LCD screen.....hence making sure that TV-out also works and our LCD screen also is fully occupied to its boundaries....