Other Parts Discussed in Thread: TVP7002
Hello TI,
We are using "ezsdk_dm814x-evm_5_05_01_04" with EVM board. We are playing with various OpenMax demos available in the ezsdk. We have gone through capture_encode demo available at "component-sources/omx_05_02_00_46/examples/ti/omx/demos/" in the ezsdk. In this demo we are setting mode (720/1080p) from which we are setting capture capture parameters based that.
We do have a requirement of auto detect the video capture resolution from TVP7002 and set the capture parameters accordingly.
Can we have a quick response on this ?
Regards,
Hitesh