Other Parts Discussed in Thread: AM3352, TPS2051
I want to use one USB port on AM3352 as OTG, i.e i want it to be configurable as host or a peripheral device port . After reading the TRM , the following section :
Two options (h/w or s/w) exist for a USBrole assumption/configuration.
For a USB Peripheral configuration the user has the option of using the cable end to select the role by attaching the mini or micro b side of the cable (can consider this as a h/w option) or use the optional method where the firmware is required to program the respective USB Mode Register IDDIG bit field with a value of ‘1’ prior to the USB controller goes into session (can consider this as a s/w option).
Similarly, for a USB host configuration the user has the option of using the cable end to select the role by attaching the mini or micro a side of the cable (can consider this as a h/w option) or use the optional method where the firmware is required to program the respective USB Mode Register IDDIG bit field with a value of ‘0’ value prior to the USB controller going into session (can consider this as a s/w option).
When using the s/w option, the USB ID pin state is ignored/bypassed (this is a similar configuration where an ID pin does not exist) and the USB2.0 controller role adaptation of a host or peripheral (device) is dependent upon the state of the respective USB Mode Register IDDIG field. If the IDDIG field is programmed by the user with a value of ‘1’ prior to the USB going into session, it would assume the role of a peripheral/device. However, if the IDDIG field is programmed with the value of ‘0’, the USB controller will assume the role of a host. What this means is that the USB cable end, connector, will not be able to control the role of the OTG controller and the user needs to be aware of the firmware program setting prior to performing a USB connection.
The procedure for the USB2.0 OTG controller determining its operating modes (usb controller assuming a role of a host or a peripheral) starts when the USB 2.0 controller goes into a session. The USB 2.0 controller is in session when either it senses a voltage (>= 4.4V) on the USBx_VBUSIN pin and the controller sets its DEVCTL[SESSION] bit field or when the firmware sets the DEVCTL[SESSION] bit; assuming that it will operating as a host.
So I am in confusion as to what should i do, need some guidance .