This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is VDS(max) of the open drain HDQ pin on DM3730 processor?

Other Parts Discussed in Thread: DM3730, BQ27000, OMAP3530

Dear Forum,

The HDQ 1-wire pin (hdq_sio ball J25 on DM3730CBP)  is an open drain. However, I cannot find the specification of VDS(max) for the open-drain transistor. I guess that one can pull it up to 3.3V but I'm not entirely sure, because I have the mistral DM3730 EVM which buffers the HDQ pin with a 1.8V to 2.8V level translator. What is VDS(max) of the HDQ pin?

Yours sincerely

Stephen Blake