Dear gentlemen,
We are working on a OMAP4460 custom desing with a dual camera (ov5640 and ov2655) on an Android ICS platform. While the two cameras are working fine in Linux kernel on the MIPI bus, I am not able to export them into Android. Inside Android I could see (in the camera module) two different flavours for connecting to a camera: USB (based on V4L) and OMX. How can I configure a camera to be seen as an OMX one? And, in addition, do I need some custom ducati firmware to enable them? Any suggestion will be helpful.
Thanks a lot.
BR,
Fabio