Other Parts Discussed in Thread: AM1705, OMAP-L137, LINUXEZSDK-SITARA, DA8XX
We have custom board based on AM1705.
I compiled the latest buildroot with kernel 3.7.6 and it stops during the boot.
Here is the earlyprintk output:
___________________________________________________________________________________________
setenv bootargs "mem=32M console=ttyS2,115200n8 root=/dev/mmcblk0p1 rw noinitrd earlyprintk earlyshell debug dma_debug=on keep_bootcon memblock=debug loglevel=7 nocache nohlt noinitrd nousb apparmor=0 "
U-Boot > bootm
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.7.6
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2251632 Bytes = 2.1 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Booting Linux on physical CPU 0
[ 0.000000] Linux version 3.7.6 (root@core) (gcc version 4.7.2 (Buildroot 2013.02-rc1) ) #1 PREEMPT Wed Feb 20 16:34:56 UTC 2013
[ 0.000000] bootconsole [earlycon0] enabled
[ 0.000000] debug: skip boot console de-registration.
[ 0.000000] nocache is deprecated; use cachepolicy=buffered
[ 0.000000] memblock_reserve: [0x000000c0008400-0x000000c046e7c8] arm_memblock_init+0x4c/0x14c
[ 0.000000] memblock_reserve: [0x000000c0004000-0x000000c0008000] arm_memblock_init+0xf0/0x14c
[ 0.000000] MEMBLOCK configuration:
[ 0.000000] memory size = 0x2000000 reserved size = 0x46a3c8
[ 0.000000] memory.cnt = 0x1
[ 0.000000] memory[0x0] [0x000000c0000000-0x000000c1ffffff], 0x2000000 bytes
[ 0.000000] reserved.cnt = 0x2
[ 0.000000] reserved[0x0] [0x000000c0004000-0x000000c0007fff], 0x4000 bytes
[ 0.000000] reserved[0x1] [0x000000c0008400-0x000000c046e7c7], 0x4663c8 bytes
[ 0.000000] memblock_reserve: [0x000000c1fff000-0x000000c2000000] memblock_alloc_base_nid+0x48/0x58
[ 0.000000] memblock_reserve: [0x000000c1ffe000-0x000000c1fff000] memblock_alloc_base_nid+0x48/0x58
[ 0.000000] memblock_reserve: [0x000000c1ffdfc0-0x000000c1ffe000] memblock_alloc_base_nid+0x48/0x58
[ 0.000000] memblock_reserve: [0x000000c1ffc000-0x000000c1ffd000] memblock_alloc_base_nid+0x48/0x58
[ 0.000000] DaVinci da830/omap-l137 rev2.0 variant 0x9
[ 0.000000] memblock_reserve: [0x000000c1ffb000-0x000000c1ffc000] memblock_alloc_base_nid+0x48/0x58
[ 0.000000] memblock_reserve: [0x000000c1ffa000-0x000000c1ffb000] memblock_alloc_base_nid+0x48/0x58
[ 0.000000] Kernel command line: mem=32M console=ttyS2,115200n8 root=/dev/mmcblk0p1 rw noinitrd earlyprintk earlyshell debug dma_debug=on keep_bootcon memblock=debug loglevel=7 nocache nohlt noinitrd nousb apparmor=0
[ 0.000000] PID hash table entries: 128 (order: -3, 512 bytes)
[ 0.000000] Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Memory: 32MB = 32MB total
[ 0.000000] Memory: 27900k/27900k available, 4868k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xc2800000 - 0xff000000 ( 968 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xc2000000 ( 32 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc03f9e64 (4040 kB)
[ 0.000000] .init : 0xc03fa000 - 0xc041b11c ( 133 kB)
[ 0.000000] .data : 0xc041c000 - 0xc0446778 ( 170 kB)
[ 0.000000] .bss : 0xc044679c - 0xc046e7c8 ( 161 kB)
[ 0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] NR_IRQS:245
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.014226] Calibrating delay loop... 4.63 BogoMIPS (lpj=23168)
[ 0.149315] pid_max: default: 32768 minimum: 301
[ 0.169474] Mount-cache hash table entries: 512
[ 0.203201] CPU: Testing write buffer coherency: ok
[ 0.212237] Setting up static identity map for 0xc02f32d0 - 0xc02f3328
[ 0.346439] DaVinci: 128 gpio irqs
[ 0.396707] regulator-dummy: no parameters
[ 0.417939] NET: Registered protocol family 16
[ 0.455621] DMA: preallocated 256 KiB pool for atomic coherent allocations
________________________________________________________________________________________
any suggestion how to proceed?