Other Parts Discussed in Thread: TVP5146, TPS65930
Hi guys,
I have the DM370, DEVKIT8500D from Embest, and I want to connect the TVP5146.
My question is if I could connect the 1,8V from the TPS65930 to the TVP5146 supply. It is the same supply I am going to use with DM370.
I have the doubt if the camera could generate some noise end disturb rhe DM370.
I have noted that in the Texas EVM for DM370 they use another IC to generate the 1,8V for the camera interface.
Could I use the same supply+
Thanks in advance.