Hi,
Object: Communication PCIe DSP-DSPC6678 via the BOC
1- In the EVMs user guide, the bit 2 of switch SW9[2] if enabled (=1) indicates that Application software defined!!!
So what does it mean?? and in my case, the SW9[2] should be enabled or disabled???
2- if i want initiate PCIe transactions, the configuration of PCIe Mode should be done both in hardware(SW6) and software(PCIESSMODE=0x10 in the DEVSTAT register) or just in hardware.
and if i made 2 diffrentvalues, which will be confidered (hard or soft config)
Thank’s