Hi,
I have the questions for "Sitara SDK 5.06.00" and the included compiler.
Could you answer the following questions?
1. I'm using "AM335x Starter Kit", and I found that the SDK include "arm-arago-linux-gnueabi" compiler instead of "Sourcery G++".
Which compiler is recommended?
Now, is the use of "arm-arago-linux-gnueabi" recommended to cross-compile?
2. Can the "arm-arago-linux-gnueabi" compiler generate the "Jazelle RCT" instruction set and the "Thumb-2EE" instruction set?
If so, could you teach me the usage and the options to generate "Jazelle RCT" and "Thumb-2EE" instruction set?
If not so, and if you know, could you teach me the recommended compiler supporting "Jazelle RCT" and "Thumb-2EE"?
3. I found that "Sitara SDK 5.06.00" includes the two sets of the source codes for linux ans uboot.
- linux
~/ti-sdk-am335x-evm-05.06.00.00/board-support/linux-3.2.0-psp05.06.00.00
~/ti-sdk-am335x-evm-05.06.00.00/board-support/board-port-labs/sitara-board-port-linux
- uboot
~/ti-sdk-am335x-evm-05.06.00.00/board-support/u-boot-2012.10-psp05.06.00.00
~/ti-sdk-am335x-evm-05.06.00.00/board-support/board-port-labs/sitara-board-port-uboot
What are the differences between two sets of the source codes for linux and uboot?
Thanks
Nomoto