Other Parts Discussed in Thread: OMAPL138
Hello.
I would like to use PWRM module on OMAPL138 custom board.
There are two descriptions on material.
- C:\Program Files\Texas Instruments\pspdrivers_01_30_01\docs\OMAPL138
OMAPL138_BIOSPSP_Userguide.pdf
(P21) Please note that DSP/BIOSTM based power management support is
currently for C6748 and OMAPL138 based platform only and only BIOS
power management must be used for these platforms.
- spru423i (P121) The PWRM module is currently available for the ’C5509A
EVM and the C6748 EVM. Partial support for other ’C55x devices is also available.
Questions:
1. Does the DSP/BIOS v5.42 PWRM module support OMAPL138?
If yes,
2. Although there are PWRM libraries for EVM6748
(pscl_cfg_evm6748.a674, pmi_ctl_evm6748.a674), I can not find them for OMAPL138.
Can I use them(pscl_cfg_evm6748.a674, pmi_ctl_evm6748.a674) as for OMAPL138?
3. And, are there any methods for rebuilding libraries for OMAPL138?
Best regards, RY