hi all,
I have been using beaglebone A6 type. I have edited the ehrpwm_haptics in StarterWare2.00.00.07. I hope the PWM pulse output and ePWM2INT ISR routine. However, the delay interrupt is generated. After the event trigger is generated, the delay time is 8 ~ 10US. the interrupt routine, GPIO LED is toggled. What is the problem?
All Setting value is below.
Freq : 10MHZ, Period : 400, CMPB : 300
Output Freq : 25Khz, t : 40us
TBCTL : FREE,SOFT(1), PHSDIR(0),CLKDIV(0),HSPCLKDIV(5),SWFSYNC(0),
SYNCOSEL(0),PRDLD(1),PHSEN(0),CTRMODE(0)
TBPHS : 0
TBPRD : 400
CMPCTL : SHDWBMODE(1), LOADBMODE(3)
CMPB : 300
AQCTLB : CBU(1) - Clear, ZRO(2) - Set
ETSEL : 1 (TBCNT : 0000)
ETPS :1 (first Event)
DB : Disable
Chopper : Disable
TZ : Disable
HR : DIsable