This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About VIP configuration

I'm using vip0 parser portA to capture single 16bit yuv 422 video , vip1 to capture 8 bit video, they are both embed sync.

Vip1 works but vip0 not.

Register:

Vip0 main (address offset 0x5500): 0x1

Vip0 portA (address offset 0x5504): 0xa110

Vip0 fiq status (address offset 0x551c): 0x30004, and some time it was 0x0, or 0x4

So, is there anything I can do to fix the problem?

Thanks and regards,

maxwell