Dear all,
I have bought Chassaing's book "Digital Signal Processing and Applications with the C6713 and C6416 DSK". I'm sure a lot of you heard about it. It also includes some very use full examples for the kit mentioned in this book. I would like to know if these can be ported to the BeagleBoard-xM. What I mean is if the board is capable of being programmed with CCS and operate without an OS like Linux, etc, to do specific tasks.
If it's possible, can some one tell me if any initialization code is needed for the board to work as a standalone?