This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Some Problem about using nand flash on DM8168 evm baord

Hi all:

I use dvrrdk 2.80 on dm8168 evm board,

I have four questions about nand flash on DM8168 evm baord:

1. when my board is power on, a few minutues later the follow infomation will print out

"Read of newly-erased block at  0x077e0000 failed :-74.Putting on bad_list

Read of newly-erased block at  0x077e0000 failed :-74.Putting on bad_list

JFSS2: marking eraseblock at 0x077e0000 as bad block"

and when time goes on another new  bad block will appear again

so how it happens then how to deal with this problem?

2.I see that in the uboot HW ECC 8 is used,

   can i use sw ECC(nandecc sw), as when i flash u-boot from u-boot  into nand flash,

"mtd->read(0x800 bytes from 0x2d90800) returned ECC error"

or bad CRC found using default ,somethjng like that,

my question is taht how to select ECC  type for uboot, uImage, filesystem, it seems there different?

3.sometimes the jffs2 system will show that CRC error,

"check_node_data():wrong data CRC" Does it nomally ?

4.when the jffs2 system is in using will it read and write the nand flash all the time as i do not have my action on the jffs2 system?

best regards

xavier