Factory Apps,
Would you please review the e-mail below from an engineer at Harris and comment?
----------------
- We are trying to isolate when the issue occurs. We check the NMI pin prior to applying power, there is no short. In order to program the UCD9222 device, the +3.3V is on. All other voltages to the DM8168 processor are off. After programming the UCD9222, power is applied with the normal sequence: 3.3V, CVDD (1-V AVS) ,1-V Constant, 1.8V, 1.5V, 0.9V. JTAG testing reveals a short at that port. Power is removed to measure the NMI pin to ground and +3.3V plane. Five (5) cards have failed with this issue. Three (3) of the 5 the NMI is short to ground and two (2) of the 5 are short to +3.3V plane.
Why this pin? The pin is externally pulled up to +3.3V through 10k resistor. This is why I am asking for the IO structure behind the pin.
----------------
Thank you,
Tim