Dear sir or madam,
we are planing to run on the AM335x ICE Board the complete SysBios system (MLO and app) out of the MMC card. Which bootloader example do I have to generate and use for MLO?
1.) AM335x sysbios indusrial SDK 1.0.0.6 -> starterware -> bootloader, is this the correct one?
2.) Which address (hex value) do I have to use in the tiimage.exe to generate the correct header? (command: "tiimage 0x402F0400 MMCSD boot.bin MLO")
I've tried it on an ICE which was modified to boot from MMC and SPI has no effect (changed resistor matrix for boot config) - but this steps I've discribed above doesn't work.
3.) Is there a possibility to flash a MLO via MMC booted system to the SPI flash?
Best regards,
Matthias Boehmer