This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Scaling or resizing Display: WINCE 6.0

Other Parts Discussed in Thread: OMAP3530

hi...

we r using omap3530 under wince6.0...

we have successfully configured the display drivers for the resolution 800*600...... we have configured it to this particular resolution since we want to use TV-out and TV-out supports a max resolution of 800*600.and we also succeeded in getting the TV-out work :)

we also succeeded in displaying on both LCD display and TV-out simultaneously.. :) but the problem now is we r having a LCD display of size 1024*600....

since our build resolution is 800*600 ,we get our LCD filled only 75% of its size(1024*600)....so we want our LCD screen to be filled completely...

so how can we SCALE the 800*600 resolution to 1024*600 so that it fits our LCD screen.....hence making sure that TV-out also works and our LCD screen also is fully occupied to its boundaries....

  • as per my knowledge i dnt think we can exceed 800*600 resolution for TV-out... its clear in documentation given by TI.... but our LCD display is 1024*600.... so i wanted to stretch(scale or resize) this 800*600 resolution to 1024*600 so that it fits display exactly as well as it can be displayed on TV... :)