This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

question about log in DVRRDK_03.

Hi friends,
  As I boot in DM816x, I see both syslogd/klogd were executed

root@dm816x:/proc# top
Mem: 15044K used, 219044K free, 0K shrd, 0K buff, 6792K cached
CPU:   0% usr   0% sys   0% nic 100% idle   0% io   0% irq   0% sirq
Load average: 0.00 0.01 0.01 1/45 1075
  PID  PPID USER     STAT   VSZ %MEM %CPU COMMAND
 1069  1067 root     S     3652   2%   0% -sh
 1031     1 messageb S     3324   1%   0% /usr/bin/dbus-daemon --system
 1043     1 root     S     3000   1%   0% /sbin/syslogd -n -C64 -m 20
 1045     1 root     S     2936   1%   0% /sbin/klogd -n


   And I want to find /var/log/messages and found nothing
   So I try below and found nothing was logged.

root@dm816x:/proc# ls -l 1043/fd/
lrwx------    1 root     root           64 Apr 11 10:19 0 -> /dev/null
lrwx------    1 root     root           64 Apr 11 10:19 1 -> /dev/null
lrwx------    1 root     root           64 Apr 11 10:19 2 -> /dev/null
lrwx------    1 root     root           64 Apr 11 10:19 3 -> socket:[3404]
root@dm816x:/proc# ls -l 1045/fd/
lrwx------    1 root     root           64 Apr 11 10:20 0 -> /dev/null
lrwx------    1 root     root           64 Apr 11 10:20 1 -> /dev/null
lrwx------    1 root     root           64 Apr 11 10:20 2 -> /dev/null
lrwx------    1 root     root           64 Apr 11 10:20 3 -> socket:[3411]
root@dm816x:/proc#

   Does anyone knows how to enable the log?