Other Parts Discussed in Thread: AM3894
Hi,
I have these long PCIe traces, about 6 to 7 inches, running on my AM3894 custom board which I am not able to get the PCIe link up.
I am connecting the PCIE to a FPGA with just a single lane. So far, from the register 0x51001728, I keep getting 00 at bit 1 and 0 with once a while the bit 0 toggle to 1.
Are there any adjustments like TX amplitude swing, pre-emphasis, equalization which I can tweak with?
Please advise.
Thanks and regards,
pb