Other Parts Discussed in Thread: OMAP-L138, TPS65070
Hi, I am doing (I am in the design stage) a platform with the omap-l138 but I don't know how connect the jtag's bus because I can't find a dongle jtag-usb, I have read about xds100v2, but I couldn't find information about it, I just want to find the way to use the jtag port but my computer doesn't have serial port, but it has usb port, so, Anybody can tell me a way?, becuase I want to debug with the jtag interface or, Can I debug with the uart port?
another question is that I am using the tps65070 I.C. to power the omap, and to interface with the touch-screen, but the tps65070 has and interrupt pin called int#, so I wonder if I can connect the pin int# of the tps65070 with the pin nmi# of the processor in order to handle the touch-screen information, because it seems like the pin nmi# isn't used like a normal interrupt, is it like any other interrupt (obviously active low)?, it seems to be a D.S.P. wake up interrupt but I don't know if I can use it in the way I need with the tps65070
thanks,
Daniel