This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Busybox in DVRRDK

Hi TI friends,
  Is it possible for TI to provide busybox code, because we dont know TI's configuration about this. And we just want to add several commands.
Could TI do that? I need that for DVRRDK_3.0.0.0

  • There is no specific TI configuration required.

    Refer docs/DM81xx_DVR_RDK_Minimal_Root_FS.pdf & ti810x_dvr/nfs_DM810x_UD_DVR_Min_FS.tar.lzma in 3.50 DVR RDK release for more details.

  • Thanks. Sivagamy,

    Minimal Root File System
        In DVR RDK, a minimal file system is created using busybox. DVR RDK release has this minimal file system based
        on busybox + glibc. Busybox version used is 1.20.2.(http:/ / busybox. net/ downloads/ busybox-1. 20. 2. tar. bz2)
        The release package includes the file system and ubifs image including the binaries for DM810x platform.
    File System Creation
    • Busybox package was built with default configuration.