This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCP: Retransmit Timeout

Hi everyone

 I use the ndk_2_22_01_14 and  the nsp_1_10_01_06  in the context of sys/bios.I use  the  XGCONF for configuration.when i test the ndk_evm6748_coff_helloWorld.It can works fine.But when i modify the following code  use  tcp  protocol .Connect it in client side  and send data one time .the message  TCP: Retransmit Timeout  occurs.what can i do to solve this problem.

void netOpenHook() {     // Create our local server  

 htcp = DaemonNew( SOCK_STREAMNC, 0, 7, dtask_tcp_datasrv,       OS_TASKPRINORM, OS_TASKSTKNORM, 0, 3 );

}

void netCloseHook() {    

                                   DaemonFree( htcp );

                           }

 

int dtask_tcp_datasrv( SOCKET s, UINT32 unused )

{  struct timeval to;  int I;  char *pBuf;  HANDLE hBuffer;

 (void)unused;  // Configure our socket timeout to be 5 seconds

 to.tv_sec =3;

  to.tv_usec = 0;

 setsockopt( s, SOL_SOCKET, SO_SNDTIMEO, &to, sizeof(to) );  

setsockopt( s, SOL_SOCKET, SO_RCVTIMEO, &to, sizeof(to) );

 I = 1;  

setsockopt( s, IPPROTO_TCP, TCP_NOPUSH, &I, 4 );

 for(;;)

 {  

 I = (int)recvnc( s, (void **)&pBuf, 0, &hBuffer );

  // If we read data, echo it back   

           if(I > 0)   

               {   

                      if(send( s, pBuf, I, 0) < 0 )     break;  

                             recvncfree( hBuffer );

               }   // If the connection got an error or disconnect, close  

             else    break;

             }

          fdClose( s );

     // Return "0" since we closed the socket  

   return(0);

 }

 

Using default MAC address Using MAC Address: 00-08-ee-03-14-99

MAC Address = 00-08-ee-03-14-99

EMAC should be up and running

Network Added: If-1:192.168.0.139

 �Link Status: 100Mb/s Full Duplex on PHY 0

 00015.200 TCP: Retransmit Timeout

Network Removed: If-1:192.168.0.139