This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

two questions about dm8148 boot and ddr3 config



two questions about dm8148 boot and ddr3 config.


First, when I change the bootmode from 10010 to 00001, the nandwriter project works abnormal. It cann't read and write the flash. Is it a bug or something else?

Second, when I change the uboot.min ddr clock from 400Mhz to 200Mhz,  I cann't connect the device through jtag. It stuckes in the following step when jtag start to config the ddr pll.

while (( (RD_MEM_32(Base_Address+STATUS)) & 0x00000600) != 0x00000600);

The uboot ddr clock that I change is:
../arch-ti81xx/clock_ti814x.h
#define DDR_M (pg_val_ti814x(400, 400))             //#define DDR_M (pg_val_ti814x(800, 800))

I follow this message to change the ddr clock
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/p/245226/862133.aspx#862133

What could be wrong ?

Please help me, thanks!