This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using additional peripherals with AM335x Starter Kit

I am using the AM335x Starter Kit with Android 4.2 (ICS), and looking to do some data logging type application.  My question is whether I can use the J11 pins within an Android application to talk to external SPI devices, like additional accelerometers or other sensors.

From what I can gather, I'll need to use the Android NDK and pinmuxing tool to get this communication, but documentation is a bit unclear and I don't want to dive into those two tools if it's not necessary.

Hoping somebody can quickly confirm or deny this method of using those pins.

Thanks!