Other Parts Discussed in Thread: RM48L952, CCSTUDIO
Hello!
we are prototyping a board based on RM48L952 to obtain IEC 61508 certification (SIL 3).
In order to perform the project analysis I need to know:
1) CCStudio has an embedded real time DSP/BIOS kernel. Is this kernel IEC 61850 certificable? Has got CCStudio the kernel source code ? Is it obtainable ?
2) May I plan to write a program without using DSP/BIOS kernel ?
3) Can I use all the CCStudio features (debug, profiler, configuration etc.) without the kernel ?
Thanks in advance
Marcello Dechirico