This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x GPMC burst behavior

Hi,

I would like clarification on the TRM statement "required accesses", i.e how it affects the case of residue words that does not fill a complete burst.

7.1.3.3.10.5 System Burst Versus External Device Burst Support 
“When the system burst request length is less than the ATTACHEDDEVICEPAGELENGTH value, the GPMC proceeds with the required accesses.”

1- If I have setup the GPMC to run NOR Synchronous 4x 16bit word write bursts, then launch a write from DMA as 10x 16bit words to the memory, what access mode will the GPMC switch to for the last two words?

2- What timing penalty occurs (bus turn-around time)?  

Thanks.

/Magnus