Hi,
I am referring to this document - http://www.omappedia.com/wiki/4AI.1.7_OMAP4_Icecream_Sandwich_Release_Notes
I can successfully build u-boot and x-loader and now I am trying to build the kernel using the following command -
make ARCH=arm distclean
make ARCH=arm blaze_defconfig
make ARCH=arm uImage 2>&1 |tee ${MYDROID}/logs/kernel_make.out
But I am getting the following error -
cripts/kconfig/conf --silentoldconfig Kconfig
CHK include/linux/version.h
UPD include/linux/version.h
CHK include/generated/utsrelease.h
UPD include/generated/utsrelease.h
Generating include/generated/mach-types.h
CC kernel/bounds.s
gcc: error: unrecognized command line option ‘-mlittle-endian’
gcc: error: unrecognized command line option ‘-mapcs’
gcc: error: unrecognized command line option ‘-mno-sched-prolog’
gcc: error: unrecognized argument in option ‘-mabi=aapcs-linux’
gcc: note: valid arguments to ‘-mabi=’ are: ms sysv
gcc: error: unrecognized command line option ‘-mno-thumb-interwork’
make[1]: *** [kernel/bounds.s] Error 1
make: *** [prepare0] Error 2
I am not sure what this means? Am I missing some libraries to be installed?
Thanks in advance
-Palak