This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IMX036 sensor driver on IPNC

Other Parts Discussed in Thread: DM385

Hi,

 HW: DM8127
 SW: ipnc_rdk_v3.2

 I am looking to develop IMX036 sensor driver on the above mentioned platform. This IMX036 supports SPI.

  1.  Can we use IMX136 SPI driver in ipnc_rdk_v3.2 as a reference for this activity(since both sensor need SPI) ?
  2. If answer to above question is yes, then Can we migrate the same IMX036 driver on ipnc_rdk_v3.2 to rdk_v3.5 without any changes?

Appreciate your help.