This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD card boot problem



Hi

We have just moved from our prototype stage and into production. During production test we have noticed a problem affecting a single board.

During the Linux boot phase the Kernel panics and it is almost certainly due to this:

Waiting for root device /dev/mmcblk0p2...
mmc0: new high speed SDHC card at address e624
mmcblk0: mmc0:e624 SU08G 7.40 GiB (ro)                           <=========== READ ONLY
mmcblk0: p1 p2
VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)

We are using a microSD card which does not have the write protect pin. The WP pin on the DM8168 is left unconnected so should thus have a logic low due to the IPD which is enabled. There is no errata for this problem so I'm not sure what to conclude.

If I use CCS and change the PINCTRL for the WP pin to GPIO, then I can see that it is at a logic low. I can do the same for the CD (card detect) pin and can observe that this changes state when the card is removed.

I have also Googled the error "cannot open root device mmcblk0p2 or unknown-block(179 2)" and Google knows this phrase and points to these forums where others have had the same problem. The solution, as far as I can tell, seems to be to replace the EVM in those cases. That would imply a "dead" DM8168?!

What are your thoughts on this? Is this indicative of a faulty device?

Thanks.

  • Hi Graeme,

    Are you on EZSDK? If yes, what version? What is the silicon revision of your DM816x device?

    This looks to me like your root file system is damaged. Can you confirm that your /media/ROOTFS partition is fine (can be mounted on the Ubuntu PC, and contain all the needed files and folders, like /bin, /boot, /etc, linuxrc, etc.)

    Also post your boot arguments.

    Regards,

    Pavel

  • Hi Pavel

    Yes, we're using EZSDK version 5..05.

    I'm not sure it does show a corrupted file system as the same microSD card works fine in all of our other boards. In fact, I've just tried another (working) microSD card with a different build of Linux and that also shows exactly the same problem (but also works ok in our other boards).

  • Sorry, it's silicon version 1.1

  • I made a try with my own micro SD card and DM816x/AM389x EVM.

    1. When I try with the locked micro SD card, I have the same as you:

    Waiting for root device /dev/mmcblk0p2...
    mmc0: new high speed SDHC card at address 0002
    mmcblk0: mmc0:0002 00000 3.70 GiB (ro)
     mmcblk0: p1 p2
    VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)
    Please append a correct "root=" boot option; here are the available partitions:
    1f00             256 mtdblock0  (driver?)
    1f01               8 mtdblock1  (driver?)
    1f02            2560 mtdblock2  (driver?)
    1f03            1272 mtdblock3  (driver?)
    1f04            2432 mtdblock4  (driver?)
    1f05             128 mtdblock5  (driver?)
    1f06            4352 mtdblock6  (driver?)
    1f07          204928 mtdblock7  (driver?)
    1f08           50304 mtdblock8  (driver?)
    b300         3880960 mmcblk0  driver: mmcblk
      b301           40131 mmcblk0p1 00000000-0000-0000-0000-000000000mmcblk0p1
      b302         3839535 mmcblk0p2 00000000-0000-0000-0000-000000000mmcblk0p2
    Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
    Backtrace:
    [<c004abb8>] (dump_backtrace+0x0/0x110) from [<c039d918>] (dump_stack+0x18/0x1c)
     r7:d6414000 r6:00000000 r5:c002ec44 r4:c0523750
    [<c039d900>] (dump_stack+0x0/0x1c) from [<c039d97c>] (panic+0x60/0x17c)
    [<c039d91c>] (panic+0x0/0x17c) from [<c00092b4>] (mount_block_root+0x1e0/0x220)
     r3:00000000 r2:00000000 r1:d643bf58 r0:c045c03c
    [<c00090d4>] (mount_block_root+0x0/0x220) from [<c00093a0>] (mount_root+0xac/0xcc)
    [<c00092f4>] (mount_root+0x0/0xcc) from [<c0009530>] (prepare_namespace+0x170/0x1d4)
     r4:c0522f64
    [<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154)
     r5:c00086b0 r4:c0522f00
    [<c00086b0>] (kernel_init+0x0/0x154) from [<c0072df4>] (do_exit+0x0/0x5e4)
     r5:c00086b0 r4:00000000

    2. When I try with not locked micro SD card, everything works fine:

    Waiting for root device /dev/mmcblk0p2...
    mmc0: new high speed SDHC card at address 0002
    mmcblk0: mmc0:0002 00000 3.70 GiB
     mmcblk0: p1 p2
    EXT3-fs: barriers not enabled
    kjournald starting.  Commit interval 5 seconds
    EXT3-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
    EXT3-fs (mmcblk0p2): using internal journal
    EXT3-fs (mmcblk0p2): recovery complete
    EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
    VFS: Mounted root (ext3 filesystem) on device 179:2.

    So you need to double check that the micro SD card is not locked.

    When I locked my own micro SD card, I can not mount the ROOTFS on my Desktop Ubuntu PC, I have "Unable to mount ROOTFS". Can you try if you can mount your root file system? If you are using the EZSDK script, it should has the name ROOTFS and available under /media/ROOTFS when you plug the micro SD in your card reader.

    Best Regards,

    Pavel


  • Hi

    Thanks.That's good news - sort of!

    Yes, when I plug the card into my PC the rootfs can be mounted.

    How do you lock your microSD card?

  • I plug my micro SD card into a micro SD adapter. And in this adapter, I have a switch, named "LOCK", and I use this switch to lock and unlock the micro SD card. See the picture: http://www.iltelefoninoofferte.it/index.php?main_page=popup_image&pID=703&zenid=eac7175d323ac3c4877a10c9520b0ca3

    Can you try to use root file system not from SD card, but from NFS or Flash (NAND, NOR, SPI). Thus we will be sure that the problem is in the MMC/SD controller peripheral module.

    Best Regards,

    Pavel

  • I have made one more experiment.

    1 case - when SD card is not locked. In this case, when I interrupt the boot process in the u-boot stage and then I read the SD_SYSTEST (0x48060128) and SD_PSTATE (0x48060224) I have the following values:

    TI8168_EVM#md 0x48060128
    48060128: 00000000 00000000 00000000 00000000    ................


    TI8168_EVM#md 0x48060224
    48060224: 01f70000 00000d02 000e0007 20008002    ...............

    2 case - when SD card is locked:

    TI8168_EVM#md 0x48060128
    48060128: 00004000 00000000 00000000 00000000    .@..............

    TI8168_EVM#md 0x48060224
    48060224: 01ff0000 00000d02 000e0007 20008002    ...............

    Could you please provide your SD_SYSTEST and SD_PSTATE values in u-boot?

    Regards,

    Pavel

  • Thanks. Here are the results:

    TI8168_EVM#md 0x48060128
    48060128: 00000000 00000000 00000000 00000000 ................

    TI8168_EVM#md 0x48060224
    48060224: 01f70000 00000d02 000e0007 20008002 ...............

  • It seams there are differences between micro SD card and standard SD card regarding the WP pin:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/249400/873354.aspx#873354

    Regards,

    Pavel

  • Hi

    Thanks for the link.

    I've read through that thread but honestly I'm not sure what their problem was.

    It looks like their issue might be due to the WP pin not being used or driven to the wrong state when using a microSD card.

    I'm not sure that applies in my case. We are leaving the IPD of the WP pin to enable write access to the card. We have 13 boards built now and two suffer from the microSD (ro) problem.

    I'm going to look at the Linux SD card driver and see if I can remove the WP link.

  • Not being a seasoned Linux s/w developer, where would you look to find the sources of the SD card driver?

  • One more thing. I noticed on these forums that another person has had the same fault:

    http://e2e.ti.com/support/embedded/linux/f/354/t/177933.aspx 

    ("Getting error "VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)" while booting from SD card, DVSDK 4.X, platform: DM36X")

    The solution here was to replace the EVM. Do you have a record of this replacement and if the faulty EVM was investigated further?

  • Hello,

    Graeme Parker said:
    where would you look to find the sources of the SD card driver?

    For the MMC/SD driver check:

    http://processors.wiki.ti.com/index.php/TI81XX_PSP_MMC_SD_Driver_User_Guide

    ti-ezsdk_dm816x-evm_5_05_02_00/board-support/linux-2.6.37-psp04.04.00.01/drivers/mmc

    BR,

    Pavel

  • Thanks. Of course now I have another question.

    I downloaded ezsdk_dm816x-evm_5_05_02_00_setuplinux and installed this on my Ubuntu PC.

    After installation is complete I do not have this location ti-ezsdk_dm816x-evm_5_05_02_00/board-support/linux-2.6.37-psp04.04.00.01/drivers/mmc

    The only folder in board-support is u-boot-2010.06-psp04.04.00.01

    Is there something else I should download?

  • You should go to this page: http://software-dl.ti.com/dsps/dsps_public_sw/ezsdk/latest/index_FDS.html   

    Then you should download the ezsdk_dm816x-evm_5_05_02_00_setuplinux bin file and place it in your HOME directory on your Ubuntu 10.04 LTS 32-bit or Ubuntu 11.10 32-bit PC.

    You should install the CodeSourcery tool chain, as per instructions in this web page: ./arm-2009q1-203-arm-none-linux-gnueabi.bin

    If necessary make the installer executable manually by executing:

        chmod +x ezsdk_dm816x-evm_5_05_02_00_setuplinux

    Execute the installer on the host and follow the instructions:
        ./ezsdk_dm816x-evm_5_05_02_00_setuplinux

    At the end of the installation, you should have the ti-ezsdk_dm816x-evm_5_05_02_00/board-support/linux-2.6.37-psp04.04.00.01 folder in your HOME directory.

    Regards,
    Pavel
  • Thanks.

    I now have my Ubuntu PC setup and am able to run: make linux, make linux_install, make u-boot and make u-boot_install. And I can run the mksdboot.sh script too.

    I have found the section in the SDcard driver source that I believe could provide a workaround to the read-only problem.

    But, from what I can tell, mksdboot.sh is trying to get files from \usr\local\ezsdk\board-support\prebuilt-images, but this is not where the results of the make are. Is there a proper guide to rebuilding the Linux kernel, rebuilding u-boot, and making an SDcard?

    To be honest, it's a complicated makefile and I'm not sure where the results are made. Where are MLO, u-boot.bin and uImage? I do know that a copy ends up in \home\<user-name>\targetfs\home\root\dm816x-evm\boot. Should I just use these for the SD-card?

  • Graeme,

    You can create SD card with the script. Then you can replace the pre-built MLO, u-boot.bin and uImage with the new generated ones.

    For how to create/make/build new MLO and u-boot.bin, check the U-Boot User Guide: http://processors.wiki.ti.com/index.php/TI81XX_PSP_U-Boot

    For how to create/make/build new uImage, check the PSP User Guide: http://processors.wiki.ti.com/index.php/TI81XX_PSP_User_Guide#Linux_Kernel

    The new generated MLO and u-boot.bin are in ti-ezsdk_dm816x-evm_5_05_02_00/board-support/u-boot-2010.06-psp04.04.00.01

    The new generated uImage is in ti-ezsdk_dm816x-evm_5_05_02_00/board-support/linux-2.6.37-psp04.04.00.01/arch/arm/boot

    Regards,

    Pavel

  • Hi

    I've modified the sd.c file to always return FALSE for the read-only check. Now the board works perfectly!

    Putting the original read-only check back into the kernel causes the Linux boot procedure to fail as before saying that the file system is (ro). So I'm pretty sure I'm on the right track.

    I should investigate further within the sd.c (and associated) files to find exactly where the fault lies. To me, at this point, it would appear to be faulty silicon.

  • Graeme,

        We have a board based on the DM8168 that has been in production for about a year.  We have a configuration that sounds identical to yours: microSD card with the WP pin on the 8168 left unconnected.  Recently, the microSD card that we had been using went EOL and in the process of qualifying a new microSD card, we stumbled across this problem with the read only filesystem.  At this point we are going to try to repeat your experiment with the changes to sd.c to force the return to always be FALSE.  That said, you indicated in this thread that you were going to do some further research to try to get to the root cause of the failure.  Did you ever complete that research?

    Thank you in advance for your help,

    Mike Kahn

  • Hi,

    I am also facing the same issue with my custom board using DM8168 and EZSDK 5.5.2.
    Im able to do nfs booting, But stuck on the same place as mentioned in the post when using sd card booting. Anybody able to resolve this issue.
  • Sorry for such a very late response.

    No, I never made any further progress as the change I made worked - so we shipped it!

  • Hi,
    No, not resolved. I just continued with the fix I found by modifying sd.c
  • Hi Graeme Parker,

    Thanks for the responce.

    What fix? That fix will work only for the affected board right. For rest of the board you are having another   build images

  • The problem I had was that the filesystem was ro.
    I modified the sd.c file (in drivers/mmc/core/sd.c) to always return FALSE for the read-only check. Now the board works perfectly!
    Around line 500:
    /*
    commented out to ignore ro bug GP120313
    if (!reinit) {
    int ro = -1;

    if (host->ops->get_ro)
    ro = host->ops->get_ro(host);

    if (ro < 0) {
    printk(KERN_WARNING "%s: host does not "
    "support reading read-only "
    "switch. assuming write-enable.\n",
    mmc_hostname(host));
    } else if (ro > 0) {
    mmc_card_set_readonly(card);
    }
    }
    */
    It was 4 years ago.
  • Hi Graeme Parker,

    This code change worked with our board also. Only one board was having this issue and we kept it for development purpose.