Hi,
I want to use one of the 32 bit timers on the 6748 to calculate the time difference between 2 seperate interrupts. The time difference needs to be within 10's of ns. I configured Timer1 to be 32 bit unchained continuous. I set the period for max value. I set up the timer to reset when TIM12 is read. I read the TIM12 register, perform 3 NOP's and then re-read the TIM12 register again and the values don't seem reasonable. I am using SYS/BIOS. Basically I want to be able to clear the clock counter. Start the clock counter when I receive the first interrupt and then stop and read the clock counter results when I receive the second interrupt.
Thanks,
Will