Other Parts Discussed in Thread: AM3517
Hello,
I'm currently having trouble with our TI AM3517 CE6.0 device's ethernet performance.
In detail, WinSock API function recvfrom() (non-blocking mode) has a very long duration (1-3ms).
I compared it to our other CE-based devices:
- Win CE5.0 / XScale PXA270 / Keith&Koepp BSP
- Win CE6.0 / AT91 platform / adeneo BSP
Here, recvfrom() takes less than 1ms.
As the PUBLIC and PRIVATE sources are the same, I assume the ethernet driver in the
TI BSP isn't very well optimized.
Has anyone a solution for this problem?
Or is there an optimized ethernet driver for the AM3517 platform available?
Thanks in advance for any help.
Winsock recvfrom():
http://msdn.microsoft.com/en-us/library/ee494234(v=winembedded.60).aspx