Other Parts Discussed in Thread: TPS65910
Dear support team,
I have a question regarding the behaviour of the RTC with silicon rev. 2.0 of the AM335x with the following szenario:
(1) All power supplies off
(2) Cold reset of the complete system
(3) The software initializes the RTC and the system is in active mode
(4) Power loss of the main power supply, the RTC domain remains powered with a backup battery
(5) POR of the main supply, system initializes and remains in active mode
Questions:
- What happens with the system time during (4) and (5)? Is the time information lost and/or the RTC oscillator stopped during power fail or POR of the main supply?
- Is there an increased supply current of the VDDS_RTC supply because the AM335x is in "active" instead of "RTC only" mode?
Best regards
Reto