This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

init header file for coded in DSK6713?

hi...

i m using TMS320C6713 and using ccs v5.2 to load programme.

i have downloaded support file called DS6713 and chip support library from website....

i have got an error of dsk6713init.h file which is missing in my library file.......so i m not able to include it in my project,

hence i m not able to call function which are defined in header file and necessary to configure codec as well as write programme.

please tell me where can i find this?

thnx

regards

jay sompura.... 

  • Jay,

    If you have downloaded the BSL and CSL libraries, you should have everything that is available.

    What example file or document leads you to look for a file named dsk6713init.h?

    Regards,
    RandyP

  • thank u for rply..

    here, i have attached a file in which programme is written which include init.h files...

    i had downloaded it from net to know the uploading process through ccs v5.2...in dsk6713...

    1234.init.docx

    regards

    jay sompura

  • Jay,

    The filenames for the #include statements in your attached file do not match the filenames you asked about in your first post above. If you do not type the name correctly, the compiler will not find the file.

    RandyP said:
    If you have downloaded the BSL and CSL libraries, you should have everything that is available. 

    This is still true. Perhaps you have mis-typed the filename or perhaps you are referencing an incomplete project.

    RandyP said:
    What example file or document leads you to look for a file named dsk6713init.h?  

    Start by building and running an example from the CSL and/or BSL files that you downloaded. Do not modify them other than to make changes, if any, required for your version of CCS.

    If you are starting from another example or have written your own program, then there is no way to help you other than to tell you it is wrong and you need to start from one of the BSL examples exactly as it comes from the download.

    Regards,
    RandyP

  • thnx randy

    sorry for previous post...

    now i m reffering an ebook of Rulf chassing.

    so now i won't make any mistake and for difficulty, i can give u a standard refrence rather than a random coding from net.

     regards

    jay sompura

  • Jay,

    Search the E2E forum for "rulph chassaing" (no quotes) to find a number of threads that have dealt with building examples from his books. The E2E forum is very powerful in the depth and breadth of answers that have been posted, and many have been written by users like yourself who went through this process and reported back on their experiences. That is what builds such a great forum of answers, and that is what gives the most power into your hands when you visit the TI E2E Forum.

    Be sure to spell his name correctly in order to find the greatest number of positive matches.

    Regards,
    RandyP