Hi,
I'm in the market for buying a new DSP (the current is a TMS320F28335). I would like to have better ADC, memory and something to grow with and the OMAP-L138/TMS320C6748 EVM kit ($1050...) seems to have that.
1) What are the difference between all OMAP-L138/TMS320C6748 kits (see http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/232285.aspx)?
2) Is there example code that comes with the kit that utilizes the on-board 20 MSPS ADC?
3) Will the ADC and other peripherals work if I only run my code from the C6748 SOM, or is the OMAP SOM needed for some things?
4) From what I understand the OMAP is linux based. What does this mean in terms of programming? I'm used to C++ in CCS from my F28335, can this be used in the same manner if I have a C6748 SOM?