Other Parts Discussed in Thread: AM3352, AM3359
I have closely followed Beaglebone board in designing a custom board using AM3352.
I want boot order to be MMC1 - NAND- UART0- USB0- 24MHz
I understand from Table 26.7 in TRM that this boot mode is not available there. I have to use MMC1 instead of MMC0 because UART1 port is completely used, and hence a confused and staggered boot order.
I would be glad if some pointers can be provided so as to get this boot mode.