A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the recommended place to initialize DDR3 memory?
As far as I understood, DDR3 initialization could be done in boot table format by supplying an appropriate table whereas DDR3 initialization is actually done by the EVM's IBL.
Is there also a way to accomodate DDR3 initialization in a ROMFS image?
If a specific application is to be loaded to DDR3 memory and the application wants to use DDR3 settings different from those in IBL, how would one do that? I can imagine that running DDR3 at reduced speed could decrease power consumption.
regards
Guenter