Other Parts Discussed in Thread: OMAP-L132, ADS802, OMAPL138, OMAP-L138
Hi,
My customer would like to know if OMAP-L132 support a direct connection to the ADS802?
Thanks
Marcus
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Marcus,
OMAPL132 offers a subset of the features available on OMAPL138. So, please refer to below link, in which the list of
ADCs supported by OMAPL-138 is given.
But the specified "ADS802" is not mentioned.
TI offers a wide range of ADCs with different sampling rates. please refer to http://www.ti.com/lsds/ti/analog/dataconverters/adc_dac_quick_search.page to check for compatibilty.
Regards,
Shankari.
--------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------
Hi Shankari,
Can you share some thoughts on why the ADS802 is not included as a compatible device? Is it because it is 5-V logic, or because the interface is not supported (i.e. would it be supported with a level shifter)?
Thanks,
Antonio
Hi Antonio,
Suggestion from the hardware team:-
OMAP-L132 doesn't have Parallel Port (uPP) peripheral that support parallel interface for ADC,DAC & FPGA as a part of OMAP-L138.
The ADC ADS802 suggested by you has parallel interface. So, there is no way it can be interfaced with OMAP-L132 unless you've SPI or I2C based I/O ex-pander which requires 5V to 3.3V logic conversion.
And also, adding so many components to interface this ADC (AD808) and make it work is cumbersome. The better option would be to go for SPI or I2C based ADC with 3.3V logic level interface.
Regards,
Shankari.
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------