This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EtherCAT SSC 5.01 DC Hot Connect Behavior

Other Parts Discussed in Thread: AM3359

Hi,  I am using two AM3359 ICE boards running the stock 5.01 SSC 'app' file from the SD card, using TwinCat, and enabling the DC distributed clock in default automatic mode with 4 ms cyclic.

They boot up and go to OP ok, but when I disconnect the second slave in the daisy chain and reconnect it, TwinCat cannot restore the slave to OP mode, either automatically or manually, I have to power cycle the boards to get back to OP mode.  If I disconnect the first slave in the daisy chain from the master, then Twincat can restore OP mode when reconnected.

If I try this with two Beckhoff EL9800.4 demo boards running 5.01 SSC on the PIC cpu with the ET1100 ESC, I can disconnect reconnect either slave while the boards are in OP state and they will recover to OP state once reconnected.

Should the hot connect work while DC is enabled?

There is no hot connect issue when DC is off.