This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

McASP stopping external sync signals

Other Parts Discussed in Thread: AM1808

AM1808's McASP with the TDM transfer mode (I2S) is connected to the FPGA.
Sync signals are outputted by the FPGA.

FPGA may stop the output signals between data transfers.
If the ACLKX/R pin is used as the bit clock input, can the bit clock be stopped?
If the AHCLKX/R  pin is used as the high-frequency clock input and the ACLKX/R pin is not used, can the high-frequency clock be stopped?

Best regards,

Daisuke