This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Poor SSD performance on DM8148

Dear All,

I am testing SSD drive performance connected to DM8148. In my setup I use DM8148 EVM and OCZ Vertex 3 SSD drive, u-boot and Linux kernel are from PSP_04_04_00_02.

SSD drive is detected as SATA-2 device, link stays in SATA-2 mode, I do not see any errors. IO scheduling is disabled.

For the test I use something like the following command: "time dd if=/dev/null of=/dev/sda bs=1M count=5120"

On DM8148 after multiple repetitions the average speed is approximately 95MB/s.

The same drive on my Linux workstation with the same test shows 200+ MB/s.

What is the reason for such a difference in performance? Is it the hardware limitation? If not, how to improve it?

Thank you for any suggestion