This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Restoring the OMAP-L138 EVM SPI Flash

Expert 2370 points

Other Parts Discussed in Thread: OMAP-L138, OMAPL138

Hi,

I am using OMAP-L138 EVM with OMAPL138 SOM at windows platform. I flashed a simple test program using the wiki page given below which repeatedly blinks the LEDs on the OMAP-L138 EVM after booting. When I boot the EVM, LED is flashing but whenever I Debug Active Project in CCS v 4.2.0 to run other projects, I always get the following error message;

C674X_0: Error connecting to the target: Error 0x80000240/-1180 Fatal Error during: Initialization, OCS,  The target is being held in reset.  The applied reset must be released before progressing.  

which eventually goes away after pressing RESET and it debugs active project. I successfully restore the OMAP-L138 EVM SPI Flash using ubl_OMAPL138_SPI_MEM.bin file but still getting the same error message when try to debug active project.

I wonder how can I fix this problem ? How can I get the factory default setting ? Is ubl_OMAPL138_SPI_MEM.bin correct file which I flashed ?

I appreciate your help.

Thanks.

BAS