Other Parts Discussed in Thread: OMAP-L138
Hi,
I am trying to use serial flash loading utility to load a ais u-boot to a custom board that is based on a OMAP L138 logic evm board.
Using the OMAP L138 evm as first try, I wasn't able to load the u-boot.
I have all the images that came with DaVinci-PSP-SDK-03.22.00.02 [1] with:
slh_OMAP-L138.exe -waitForDevice -v u-boot-spi.ais
and don't print any message of error but when opening the serial port don't receive any output.
From texas wiki [2] page it says that to load to RAM it needs the version 2.xx but OMAP-L138_FlashAndBootUtils_2_40 brings the ./slh_OMAP-L138.exe wit version 1.65.
The guys with hawkboard [3] used this method to save the images to spi [2] so it should work ...
Any hint about this ?
[1] - ./DaVinci-PSP-SDK-03.22.00.02/images/u-boot/omapl1x8/u-boot-*.ais
[2] ̣- http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility
[3] - https://groups.google.com/forum/?fromgroups=#!topic/hawkboard/55-fy2KaJiU/discussion