This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 SD card over spi0

hi

I m stying to interface sd card over spi0 to my dm365 board

this is the log coming

mmc_spi spi0.0: ASSUMING SPI bus stays unshared!                                
mmc_spi spi0.0: ASSUMING 3.2-3.4 V slot power                                   
mmc_spi spi0.0: SD/MMC host mmc1, no WP, no poweroff

note:>there are no other logs for mmc_spi in entire bootlogs other than the above logs

the card is not detected and not registered in /dev dir to use it

i found that i m not gining any platform data for the card in spi mode

but i dont know what platform data shud be given

please clear the doubt that

1.we have to give platform data to detect the card

2.if yes then please provide it or any help related

thanks

kailash