I've got the Quad-DSPC 8681 PCIe card and could never get the SRIO working amongst the DSPs.
Anyone could show me some demo of that?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yang Gao,
Since I do not have one of these boards, I cannot say for sure. But most board vendors supply a set of example files with the delivery of the board.
Have you looked through the documentation and files that came with your board?
Have you checked the vendor's website for support files?
Regards,
RandyP
Yang,
I do not have a board here either or example code, but you should be able to use the MCSDK SRIO examples on this PCIe board. The following items will have to be addressed:
- You will have to take the example out of loopback
- You will have to modify the Serdes configuration for a 250Mhz reference clock on the PCIe card instead of the 312.5 reference clock on the EVM.
- Make sure the port width is 1X and that you are using the correct port numbers when trying to talk to adjacent DSPs on the PCIe card.
http://software-dl.ti.com/sdoemb/sdoemb_public_sw/bios_mcsdk/latest/index_FDS.html
After installing look at: C:\ti\pdk_C6678_x_x_x_x\packages\ti\drv\srio for the examples.
Regards,
Travis
Yang,
BTW, the file you will need to edit is C:\ti\pdk_C6678_1_1_2_5\packages\ti\drv\srio\device\device_srio_loopback.c
/* Configure SRIO ports to operate in loopback mode. */
CSL_SRIO_SetLoopbackMode(hSrio, 0);
CSL_SRIO_SetLoopbackMode(hSrio, 1);
CSL_SRIO_SetLoopbackMode(hSrio, 2);
CSL_SRIO_SetLoopbackMode(hSrio, 3);
change to:
/* Configure SRIO ports to operate in loopback mode. */
CSL_SRIO_SetNormalMode(hSrio, 0);
CSL_SRIO_SetNormalMode(hSrio, 1);
CSL_SRIO_SetNormalMode(hSrio, 2);
CSL_SRIO_SetNormalMode(hSrio, 3);
/* Configure the SRIO SERDES Receive Configuration. */
CSL_BootCfgSetSRIOSERDESRxConfig (0, 0x00440495);
CSL_BootCfgSetSRIOSERDESRxConfig (1, 0x00440495);
CSL_BootCfgSetSRIOSERDESRxConfig (2, 0x00440495);
CSL_BootCfgSetSRIOSERDESRxConfig (3, 0x00440495);
/* Configure the SRIO SERDES Transmit Configuration. */
CSL_BootCfgSetSRIOSERDESTxConfig (0, 0x00180795);
CSL_BootCfgSetSRIOSERDESTxConfig (1, 0x00180795);
CSL_BootCfgSetSRIOSERDESTxConfig (2, 0x00180795);
CSL_BootCfgSetSRIOSERDESTxConfig (3, 0x00180795);
needs to be adjusted based on Table 3-7 of: http://www.ti.com/lit/ug/sprugw1b/sprugw1b.pdf
This should be good for 1x port config:
/* Configure the path mode for the ports. */
for(i = 0; i < 4; i++)
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, 0);
Regards,
Travis
Hi,Travis:
1.
As to what you said above :
- Make sure the port width is 1X and that you are using the correct port numbers when trying to talk to adjacent DSPs on the PCIe card.
I agree with you.Because on DSPC8681E DSP0 only use one lane(assume it is lane0) to connect DSP1.
Meanwhile,DSP0 use lane1 to connect DSP3.like below:
DSP3<--------lane1-----> DSP0 <-----lane0----->DSP1 (Assume it is true as I don't have schematics of 8681
from advantech).
So,Does what I say above mean the same thing with what you said "Make sure that port width is 1x"?
Or,May I ask you the question why you said that Make sure that port width is 1x ? Why cannot we set port
width is 4x? What's your reason? Is your reason the same with my reason I mention above? If not what's it?
2.
If it's true that we only can use one lane or one port 1x to transfer data from DSP0 to DSP1.
How can I config the port? I still refer to what you advise :
This should be good for 1x port config:
/* Configure the path mode for the ports. */
for(i = 0; i < 4; i++)
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, 0);
I don't understand why you advise that ?
Since we only use one lane or one port 1x to transfer data from DSP0 to DSP1.Does it
need to set for(i=0;i<4;i++) ? I think that should be changed like this:
for(i=0;i<1;i++) Because you only can use one port or one lane.
I guess we cannot config SRIO one port 4x mode. Is it true? I don't know ?
Thanks!
Hi,Travis:
About the CSL_SRIO_SetPLMPortPathControlMode,I want to say more .
I run the example in the pdk1.1.2.5 for SRIO Throughput on DSPC-8681E.Although
I have passed the test and the result give the performance.But I cannot understand
why I can pass the test.By the way,I modify some obvious places such as from loopback
to Normal (device to device ) and make example suitable for DSPC 8681E to move
data between DSP0 and DSP1.Luckily, I load consumer out to DSP0 and load producer
out to DSP1 and run successfully. But I don't know why?It seems unreasonable .
1.
I note that pathmode = 4 in the example,it means that you can config full lane for transfer.
pathmode = 4; //means that one port 4x
for(i = 0; i < 4; i++)
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, pathmode);
But why such config can work successfully? I don't think you can config the SRIO
for one port 4x mode on DSPC-8681E.As I know,DSP0(c6678) has 4 lanes .But
in 8681 DSP0 only use one lane to connect DSP1 and use another lane to connect
DSP3.I am not sure DSP0 and DSP1 use lane0 or lane1 or lane2 or lane3.So do DSP0
and DSP3.But one thing is sure that the lane number which DSP0 and DSP1 connect with
cannot be four.Because DSP0 only have four lanes,the four lanes may be used for DSP1 and
DSP3.But four lanes of DSP0 cannot totally be used by DSP1.So,I believe that you cannot
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, 4) to set all the ports.Because DSP0 and
DSP1 cannot use all the lanes for transfer. Transfer Pair (DSP0-DSP1) and Transfer Pair (DSP0-DSP3)
will share all the four lanes.Anyhow,I don't believe you can set pathmode = 4.
In fact ,such config pass the SRIO test .So why?
2.
Another hand,I try to modify pathmode = 0. it meas that four 1x ports.
I believe pathmode = 0 should be suitable and wright.Still the reason I confirm above that
DSP0 and DSP1 only connect each other with one lane,Assume it is lane0.So pathmode =0.
At least it should be 1x port not 4x port.But the result is disappointed.When I modify code like below
for(i = 0; i < 4; i++)
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, 0);
The example cannot pass the test.So, Where make mistakes? Does my guess standup?
Where can I get the schematics of DSPC-8681E,So I can know how many lanes and which lanes
do DSP0 and DSP1 use .So I can config SRIO port correctly .How to treat this problem?
Who leads the bad result?
Best Regards!
David,
Sorry for the late reply, still catching up on some of the items that came in during the holidays...
David George said:So,Does what I say above mean the same thing with what you said "Make sure that port width is 1x"?
Or,May I ask you the question why you said that Make sure that port width is 1x ? Why cannot we set port
width is 4x? What's your reason? Is your reason the same with my reason I mention above? If not what's it?
Yes, it must be in 1X mode, there is physically only one TX differential pair and one RX differential pair routed between each DSP, so it only supports 1X mode. For 4X mode, all 4 RX and 4 TX differential pairs would have to be routed between the two link partner devices.
It may be helpful to look at Table 2-4 in http://www.ti.com/lit/ug/sprugw1b/sprugw1b.pdf. We only support Configuration 4, but all modes within that configuration are supported.
David George said:Since we only use one lane or one port 1x to transfer data from DSP0 to DSP1.Does it
need to set for(i=0;i<4;i++) ? I think that should be changed like this:
for(i=0;i<1;i++) Because you only can use one port or one lane.
I guess we cannot config SRIO one port 4x mode. Is it true? I don't know ?
Yes you really only need to write one register, although this register can be addressed on a per-port basis, there is only one register per path/configuration.
regards,
Travis
David George said:1.
I note that pathmode = 4 in the example,it means that you can config full lane for transfer.
pathmode = 4; //means that one port 4x
for(i = 0; i < 4; i++)
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, pathmode);But why such config can work successfully? I don't think you can config the SRIO
for one port 4x mode on DSPC-8681E.As I know,DSP0(c6678) has 4 lanes .But
in 8681 DSP0 only use one lane to connect DSP1 and use another lane to connect
DSP3.I am not sure DSP0 and DSP1 use lane0 or lane1 or lane2 or lane3.So do DSP0
and DSP3.But one thing is sure that the lane number which DSP0 and DSP1 connect with
cannot be four.Because DSP0 only have four lanes,the four lanes may be used for DSP1 and
DSP3.But four lanes of DSP0 cannot totally be used by DSP1.So,I believe that you cannot
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, 4) to set all the ports.Because DSP0 and
DSP1 cannot use all the lanes for transfer. Transfer Pair (DSP0-DSP1) and Transfer Pair (DSP0-DSP3)
will share all the four lanes.Anyhow,I don't believe you can set pathmode = 4.
In fact ,such config pass the SRIO test .So why?
Yes Path_mode = 4 means 4x port. If you spend some time reading the RapidIO Serial specification, you will see that the state machines do allow for a 4x capable port to run in 1x mode. It is a fall back, if 4x operation can't be established because of a bad lane for example, the 4x port can establish a 1x port on either lane 0 or lane 2.
David George said:Another hand,I try to modify pathmode = 0. it meas that four 1x ports.
I believe pathmode = 0 should be suitable and wright.Still the reason I confirm above that
DSP0 and DSP1 only connect each other with one lane,Assume it is lane0.So pathmode =0.
At least it should be 1x port not 4x port.But the result is disappointed.When I modify code like below
for(i = 0; i < 4; i++)
CSL_SRIO_SetPLMPortPathControlMode (hSrio, i, 0);The example cannot pass the test.So, Where make mistakes? Does my guess standup?
Where can I get the schematics of DSPC-8681E,So I can know how many lanes and which lanes
do DSP0 and DSP1 use .So I can config SRIO port correctly .How to treat this problem?
Who leads the bad result?
Not sure if you are seeing errors, or if the test you are running in this setup is not sending the packets to the write port. The schematics would have to come from Advantech directly.
Regards,
Travis