Hello.
I am gonna use DDR2 SDRAM as memory of AM1806.
I would like to ask you about deciding the parameter of DRPYC1R->RL field.
The DRPYC1R->RL portion is related elapsed time of the round trip.
Even if round trip time on our target board is 10nsec and DDR_CLK is 150MHz, I think it is calculated like below:
The Round trip board delay = round trip time on our target board / DDR_CLK
= 10nsec / 6.66nsec(DDR_CLK=150MHz) = 1.50
- On this case, which value should I set (1, or 2)?
And,
- If I set the round trip time on target board as value with the margin further than the actual value is it allowed?
Best regards, RY