This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

failing installing ti-sdk-beagleboard-05.05.01.00 on Ubuntu 12.04

Hi,

 

I am working on BeagleBoard xM for 3730.  I have bought the board last week.

I have installed VirtualBox 4.2.8 onto my Windows 7.  I have installed Ubuntu 12.04 and have sharing enabled as well as my bootable SD card visible

within Ubuntu.  I  installed ti-sdk-beagleboard-05.05.01.00  without CCS which it could find.  But still went ahead with the installation.

Then I did "./setup.sh" and it gives the below error.

               TISDK setup script

                This script will set up your development host for SDK development. Parts of this script require administrator priviliges (sudo access

                Verifying Linux host distribution Unsupported host machine, only Ubuntu 10.04 LTS supported Failed setup, aborting..

I do realize that this  ti-sdk-beagleboard-05.05.01.00  is for Ubuntu 10.04.  I was wondering if there is a way to fix this failure?

Any suggestions and help would be very much appreciated.

Thanks,

Asha