This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Writing custom links on DVR-RDK DM8168 McFW



Hi,

   I am developing NVR based on DVR-RDK, which stores videos from IPNC cameras.

   For now, I have used live555 to get the h264 encoded stream from IPNC cameras & saved the live555 captured stream to files. And then, the Dec + Dis demo of DVR-RDK reads the video file, decodes & displays the video correctly.

   However, using files as the method to transfer bitstream is not very good for the “live555 ---> decode ---> display” path. I consider to use shared memory to transfer the bitstream, & I think it is also not very good.

   I would perfer to wrap the live555 to be a customized link which looks like the capture link or encode link, so it transfers bitstreams the same as McFW links. My question is:

    (1) How can I implement the data transfer between live555 and the decoder?

    (2) Is it possible to write a custom link which implements the function of live555 & interface to the decode link (i.e. Live555Link)

    (3) Are there any demos on writing a custom link? The best news is that I can write something based on some existing demos in DVR-RDK.

Thanks

  • Hi,

         Maybe it is difficult to discuss my question.

         I found a link named NullSrcLink in DVR-RDK, could someone tell me how can I use this link? Are there any demos in DVR-RDK which uses the NullSrcLink?

         Thanks

  • NullSrcLink is for debug purposes. It acts like a captureLink but just outputs blank video frames.NullSrcLink is supported only on M3VPSS not on any other core like cortexA8.

  • Hi Badri,

           Thanks for your reply. Could you tell me how can I make a custom link which runs on cortexA8, and implements the receiv data funcion of live555 (such as we call it live555Link). So, I can connect a data flow like this:

          IPNC rtsp stream ----> live555Link on cortexA8 -----> Decoder link on m3-video ----> Display link on m3-vpss

          I just do not konw how to send live555 received h264 data to the Decoder link.

          Thank you.

  • You don't need to create a link for interfacing live555 with decode.

    You can just do

    1. Vdec_requestBitstreamBuffer

    2. Pass empty buffer to live555 stack to fill it with h264 elementary stream received from network.

    3. Vdec_putButstreamBuffer.

     

    Attached is example code to give you an idea of how this is done.(Rename attachment to .zip) The attached example is not supported and is just meant to give you an idea of how to interface with live555.Pls refer MCFW API documentation for details on how to use the Vdec APIs.

    PK�&B��e��
    rtsp_demo/demo_rtsp.c�Wao�6�\�����v�:��C��e&!`K�$;�� P$*&f�E�
    ���)ɖ�di�M@�w��ݻ��~��^x
    ��|Ɏ��2���wK�ƋA���Fq��Ns�1	i�֥b�J�
    �H5��s.�y4�wL
    �������~9|����o��s$��zr}���BC���|��ITZ�+&�yN�ZK�h��Xh�>:8�l6��\�`2TC+~S�*�AY0�
    Y��ٕ.u�T�
    �������0+�񜧉q A��L��6��Jޡ��E���h��.n!�"�����>j�}˯�7�R��sYhPL'H� '7�Θj�j!5O����%��]j[�>/L�.�bj�4��R���f%���@Uh����6<i�w�}�hW���+�,����q��V1�*}�-�a �3�0!w�E5G?,�J"U���ᆙ�%0��*3��WR3��ø�߱�F��\�U�\o̘��Ś�f�0���Tf�D5~E�.->�D�I|��ys:"#^���L/Bzz�Y0�0���t8��0�8]7��5����ӐD!��tL3��S9@}o<Q��?�-ʘNh��q���C!8�		�3����6�	�}��$-�S7��7�!Lg�4��G4��.���Y`f s������~�(8�Ih�h�C�\�ᘘ���
    ���vO
    �4ǎE��ģ��!X�^85nD���#a�N�S,��
    a��YH&�>�͆QL�YL�4FV���s���AdśE��3rc�@T]�y8��Ց�1	��4����֟�J����<�M��� �0�F�����Fc��k$�PA/n�aN��mW3��tLO����s�>��FƁ��8�wf�7�CvU�N�۱Mz�hNM	u�ED�1�zgu�7��3��m�]q_h�o��U{�*]�����u��1C��.�#��i�����
    ����Bw?�O�G[��81{�q�>�ٶ�#K���<�'}ZF<�#-׏��|��	\"po!q�>�n��q�Å�mm�LS��ɲd=[�k���[�ۊ4�����3~L$�҄�;� 6��u�#�.'��k�Og�5��uD�$W���ߙd����MO����?�_���,������e�ޯ+r���p�x��y�,�E��u�k.z
    W�5���
    ������|�yޫ��j��K��}�Y	���x��=���2�#>�UGx���di��9
    �9w��x�7�!�S-��_�-�
    ��x��l[���5ٮ�7O�D3_�w�=�.�����s��p�{����huE���<��[n��s��3�r�/�~�#r�c�.j��?�{?�o�V�������"-�?"������.��H���zu��j�9�Ob�_P�ЉҽV���F���G ��!����#���q8#O"�x�
    2�:/�:�PK�&B,���rtsp_demo/demo_rtsp.h�W[���~����K��k�g��hzC�]
    ��8��P�KkS�����T���Қ�(���;�:�<|����Ӄw�\l�'h��oe\Vj7X#ϰW��y�_��KH�]U��i���.�J�UsQ�:8�>�R�G�?
    F����}7�Ј|˿���fm�{)�Ӻ���؃�I�BUe��E��SY�d�T<��`]U�O��~�Tb�����g�Ī6Q&E�� 
    P�.Sn(+Q$��ܪ>�E�Y�����Vf"i�A��`�v�܊J�ߕ��A�N*��h��{Q<A*��$U���է�w��)����Tf(\�
    J^%�FNV�Y��� ��D��(!lO�M�O�B��&[^^�mv2s���j����4��H�LM��C�X���X�R$u̿)\G�L'J��=(�-��}��
    y�%j��aX�Y*��V\7(�R��%�q++M�P/C�y�"��nҥd^�u���j�S�z�*tS��銦���N)�O�G+ ����_P�80^"���ϗ}��0�]�,�A�t�~�����ô�%���0~t6w)����BJX�g��C��> x~hP\:�!��~��T3�S���ԥ��؜����&~`�,�[AH�ȵ�G��gt�e�k�q�Z� ^lj��i���H���c��Zc�h�&`��ud�7�n�}���Ħ���!�,�-.#��P��X3�ü�
    �R�Q@f�}L��,�ax�}�䞑`Am�����I^�H�c��qa0{(���Q�G�$�yH}�K��YB_-TwL�}O�����915��� =�96��tJf��bh��v�<�����DK��2r�%�LPc�F&|]:�)�䴱���@'`9�Ch�-m�ȤО�%hOȰ�{+����q�y<�{o���gT-]�����E
    +O��_;T��B\��K��[M�"V����zZO�l#V4t���˲8�K��ݙ�:�}"�K��UHa�sF�̽���i��z],Q��g�GqvJ�Ӣڜ&�M%�g��1.�,b�s>O��g���y.��H��_!�+��Sl
    ��%3�MyO�ӗ35|*��Z����2?���o��Lo�B	�oxZ��a2v�W$��<���,����*����ͅ�g7!�?���s<����~mv<_qp�{��J�K�џ�K���b˝Y�c�ͣ0��3�OW�������IJ�x�Pya�ԉ�sMk�e2����L��h�v��H�Gm�X3ft�p����ԉq���_⬘X���=�w�`K������h!H����<����KOK�p9'1���b�B��ޮe���n�/�!bݿi��m�=��"v8�5q�\gbb|��C4��+��t�����Qر��DD����x;���#g����u��3�*���<~s������Ɇ>�r���ٴ�A��y����&yY%��]>�~<S��h�{��HV�S�ReW�*�B�ug�"O�M6�S#��h��%-Jc�(�"��aj`�H��1��նa1�#&M?I.��Å:������Ä\�ɱ~��y��Dw%���_�~�"�fRo*7y��5�~\�aƆ^�8|~:�|��~Z�m0���b��8m�cZ�)'����S4�f{V����-q��_�ɝf�p�M=�
    Z$��ߤ뤄w�ݡ�W�FBV������F��hԺ�X��X:��PK�&B���
    �<rtsp_demo/demo_swms.c�[�sڸ���B�Nw�<l�i��h�&&i2{w<��Y���	����#ٲ��	��ٻ���s>���9G�"��[
    ���Y�–�|��3�%T��h��i6��c��p���i-MKs����,O%i�^;���\H�”r������HA��s{�i�5
    �w�^�T(���x��`t>�S�{y<��m�v��b<]K��`k���-�!��N�Trt��~���-$	������vo�w�B�k8�*j�-`R߾��`�(�q�έ6W�-�������ęq�g�РT��@,e�ug<CEW�D�5��5�{�QQ�Q[�_>��U��T7�@�U�,\�:�}�����og����<T�rR5�-@:�v�b?�87#�	Pb�8�z��	D!�T��q��lGx���,��\����4��Q��Dg���H2`�����P���(,&m5wNSP	G�!�x�0���Q_K%�Nˇ���O;+�@�p��M}v
    u˕�y���]E���nKU�!<O�����fi�Q��=��fG�z���⧺)|��(
    ���y�
    L�WO{��.R�s��ܝ�C��rZ3��B�֚�לSyh�>�l�Ls���5�=s�2mGks����$�a���
    ��|���������5%�!���!��Cp��:%��\�jz>������@��}��p��DZ	�t�~��ߏ�� '���r�k*�!�@��v�?P{������Q�k�ͱ���`$�S��ed�-�
    �4׌���Xm��]�F��.YC�1	�u�dG3�F��1��m�S*��g}�M��N�Ť�k��G;:��m	�hO ?2-�����Syq��*f��:"Np��Wl<��˝�6����P�)�?^0]�� T������~7�(��B�ުFӥ��+�1�Y��0�5�e���D��'`^�͈1,����ۇ-bj��㰣oW�/*��3�[}
    ^����y�j���m��G]�}���~����b*>0"�k2im�؅�S�+�=��$қ-ꋌ2��xjUZ�%�/~�����-j�A�Ykwn�]$�J;�N���5����$c�ҚU��F_[�f��n~��)��D��n/�" 11��^�$�"X*gقn�
    �����C}p�da�G_��QV?Ff�_��ԧzNO#�T�)��y(T}���Pqp�;R9����^��RW�-��gd��v�u}����m3v��!E��3V�'l
    ���m�ri�����*��q����Is���p��EH��Aw�z"\X�tDz���BE=f��=l��}n�ӹ	�)22��%�����YN?��b�E����l5\��Lʹ�c&�;�2LG�Dxtu%A3���	�!����S�	$@���Z�#�#�NZ#��
    ��VH=c�0�����W`��'O�ZHճJ}Z�k�y�Σ6�ˬ��Ծ����+N���(��+;8�
    7.�)��'bƇ0�ED�0���l9��\
    �&�2�~�\~g����q-��C�&�h�|M��j-%�
    �q�nw�=��U�������6_2g^ǨSyE����GY!!O@H�Qv8ۖ��pE ��W���|�H�����X��L��(���H|��dhK�/b�\�?�Z�9�{�[(���R�$.���j��C4�m��������3)a��"`:!�Tc��(��nb�aS��'�+�%��w�l�1���zh��k��S �S�����O$��k? �G':���%{�1w}��k��<0�U"	ղ������i�QL5�{L5|K����"�Bܻ�LR�����wKPr=֩B�v��#}�U���SL�G;9C�ַ"�!z߮K��+x�Q��{B�a�+\�Y��D���m�Uy�(7�_�)�_w]pv*��#�*Q㖁���
    �����Q �:"V8.mm%���"!�B����O�<�'נ$��=
    u�=Z(�ݦ{�(~?�8&J��
    TK��Ti�"�S��!Ue�v�����#Z��h����d��̉��
    �Lm��5wB�%��)�茽�$~���i�'[�#%�ev�;��������?B����!�;����Ȇy�&B�;\RH�	�$��(z�*�'��:�8��8H+y,ɶ���"ױ��6Ic򞮞�3�BG/b()�g.��SR��}��tR�a��)�7]?%z�Hh:Ă>+���YAεbE�������or�G�����v������'04�F�73����z靧�ڶc��\�l!ѿ�
    �W��n8�z��w��r�>AN訿wP����g7��׿%Q8-�7��ƛЬ�!߅��
    Qu���Mo�����ͤ���_{�3AP!���#t]�7��*�@Y��J��:�>@�����5���چ�$.$�^�-�C"����I���/���� �}[3B���B�%hC�3�4�$����;�&TbZJ,4N��j��.�
    ]��%䁸<ŝ�Pϊ��%��)�tR\��M��-��=�&��W,��H�)��� �M�Z"l!o��?PK�&B��U�	rtsp_demo/demo_swms.h��Mo�0����zI��Ҥ��S
    �A�0�vO�X
    6¦4��א�U@{Ȏ��g��!mzYp
    /i��ɋCI�2	'�54t}#��0!�*'L6�	/^ƒ��fR�5���;I��k'��v]:ϛ��Fv���!�����EM��XJv[���0BF?����+����u�6��/�|����y���Qꫭ�05�)c�Z��|�Z���H�[S���ږÔ���	�a�қ��.�m�Z(j�R�aj��Բ�����I�<b�_��S��-�)�H�C)
    ,jO<F��r���dk9H},[��w'��/�s
    ���N<y�afLt�}{_����x>Z;&Fj��S���&A\��
    |�|w�L��k���xO�['���CA:GI�W�rv��L8()��&�b2Z�YD�_ɢ�O�ޕſx%x��5�U���o2�����4���9#��Tɩ',�;�PK�&B�Fu
    3rtsp_demo/demo_vdec_vdis_rtsp.c�ks�V�;��ԙ&�N�t��B��vx�$p<mF#K�
    H�$ l����\�v�6;��Ԗ�=��=������>%x	�;Sv�c��g,mf�'�Y�an}��c��c3,s.|3k���µB�s����%�|��c�Qk�i��|�8�@	��'f+z���MB(��t��@q��_̘һ��s�7Cf�+�����^_�V�ЩYެ��5B߹]p-M׆E��q!����ȭ��ƞ?��r�	x>��-BNf���رL"R�7g��	�����hX‰����So�w`y�͍p2�8c�y"ݦ|x�D0˳x���D���y�-i*6QL��B�bU�p�"="���:�B���tf̯�/��Y&�յ(�#D�Ɣl��7���/��0C���9
    2�s��s���1� 	\s�H��z8�(�� �1��eZ�-�C=`����b	e�y!��x�g��Kfǔ�8�+����$�>�̢�CT��ҧ�s����jz[�@�_�ׂ*���H�d	Z78)��ܨ�U[�v�#ɪBO�ў�*���W5N�D���O
    ��?TYӠ���t$�T��+�V�'v��һ��^_�T:JW�T�W9�mT�_BWV�6�)�����p����#~�}�S` ��";�
    ��:�k2�����A��R
    �@� ��Z[�t�sB�랬�y��%��B�#C�������fٛ��D1;UNIȢ��md�KPo�1]M��q$�+\���#,�����%��,ڰ��>�e���%n{MVG�(k��k�xCM�đ]� ���{k�)܎JO�Uu8Е~����F+���K����ǐ�Wo�8ل��
    �m�U�1��@&�Ђ��C�h�H�Lg��W�J�2A�ҵ��t�����c` �!W�\��EN�,v�;�K��B*���7�؎]gH���q����`�C�7��ϥR��_G�0����p����Ú:X=b�����`$ɢ1�`5�ř��KU������uu(WJ�mlu�3T]@�T�&�w
    �_�[̜�,��u����#���JD��W�Wv.�'9�M��ƉAF��D��sh6~j�c�����8����=$d�<��s8)��\�J�����
    ܱа��v7ȣF���Y��ؕRd���/�)��>��4�ms]~.��v:dA���.|�eΨ.k��@�/��F~�h��U�D�R*��+�0NF&�oL?,'�����z&t5C�%�����Y	ĝ��"�⬒�E[�ݾ&("�#����5�&�O���1^���[��D/5˜2��K���yD��8Q�l=�2�S��2V� u]6
    t��$F��}���\��p\>A'���;dA�w(��n�
    �:�2��b�\����d�l,�3tD/���9�y�5-;�]�x]�!����
    ��C?�P�`���+x���sWpm׽H�_��Ek}�8�Dt316"�	���F�t��'s�Q�}�2艩O�Ь�›$Zw��av	
    j^���#2�C��D�	J{��b�gw|�܆�v~���¦���`�_P�lͬI9oL���8&�h�8OG�r��ػ�lͿ�6.�O�!��6��E�?]lp�0Nz�oO�� �o���=��
    j.��C�?J�M��"P������Vp�M��F5���­�8���
    ���Sl�s�֥O�%��b�Q֦�c�63?�,s�+V�av�!�ܾ��s��X1�hV�F��F��=�a%��F�>��ucΑ
    :R)?ϖ����@
    �B6L�dy5����&�a7>힑�{������3��:���4~Jv������B��n3\L��o %��\+c��N��	��b%0Jh��e��+�O�7��P�H����L�m<�����fdOw2v���\	D��_O)��h��ɫ��I�ɸ��uA�h�ɨU*��s ڟ�{��۹�����Fܕ�د�"�9z�%���;:S��9�	�x6p�^�o͓kGV�5o#�R�ca���U�#��5f��֭h"���]�aÍ����G��
    ����%b�ӡƍwR��.�=�j�`)�>*[3�_Q/�����{�ی�g�|]>H�J�U=����Ir�(i�%^����K��T���켏
    �尨7�3bo��׮9��j�1-�*����u��!��y��(z�g�ێ��)����~�f��uغQ|�V���5v1�WRF��oG�E
    }¸��dbA‹ǰh��m�2&_ҷt����h��YU��9(�Ҝ:6D�*}{ 
    ?Cb��˪|��F��矾�_*�ʡ��p����]n�I��[,����2%�����Sm�����Y��yλ�<2W7d�f����A���,�X��h�����/����v�Z:������������
    mRR6Jԣ�*M����yz���>�������o>��A{�	o���X{W�9$H��JSVcx��/�e��ok10_<jy����
    ���1�t6�vig��3������͖��b;�P�GF[�*k~z��P��q�@�AG�A�Kw���K���Zڒ����Zi�?�*:��&FQ�	u}��K}Mͱ���>9�QA�#�<H���T���A���<RMڐ���������51]da:
    �?&�BA�*ïTz�~8q{�B�ڞ���Qc:Y+���N����>�w̵�(��U��ر���w9��?ԍn_������Ӿ6�>vlz���u��y��ck��w
    F=m�#e���ڕ�VX쑭���Mc��a�u7�^��*�eH�x4ϲ*�4�y��~��g�W��&U3:�o1��<�jR%w^��%ʛ�5��e��7�(_�ۿ"Q��,���������7�x�v���-{(�!;&��n���/閞2���L&y
    G�'�)�� >��B�����"m�ǡ�9`�_�f�y�ܪ,�M}��Cᛁ��J�dzQd���em�a����H�+u����]A7ԫ֏g?n|�%��s*t�8.�����e� :�{�4�N=�SP�)����(��=��-����s�&���qmo80�ӭ�Մ��z�����]�,����1;ӈ�Ѯ$���ա�ܬ>
    ��r�-E�`v�~I�(E##�����t����Qhb0� �K�����>�_ǵ<���{����0aRO�'�~�|�Ԭm=٩�>ă7rP����D���"����PJ�=�}��d�!i�x�|�q£"C�'�/����<Em6e���+ko����������haN����H�I(�d�ΔSe�\gJ�-��;X��PK�&B���ԓDrtsp_demo/demo_vdec_vdis_rtsp.h�Xms�6�|���'s�_.M;u�36�1S�
    ��]����@A$�d��ޕ_{��VϮ�ݕ�t���h�+�-��`�G���u���^��Ō��E4�wأ�����M�m�r(
    ~�t����)���]'(�����Tא*k�z/�E���l���N��a�A�o����ċX#B�k�MlB��H�3h{%��B�r6������:r��%�%���l=�cY�E3T][S�����US�̳����g�|#�Qp�����d�=.�t2(�a�蚱\��t���X��Z�u~dƘ-,
    w1�/e1u²0»�0�GJv6�Ksi����؝��ա.�B1�k}9�$�sW��O��l,����q�bz����&$t��i������.��}�Tf�ք�`V��`�b8��M`�37g&-!m�Ѕ���j�Z����	ˋw�x����
    ?�e���$
    \soC�E���ǃ��L�uE��p�d05���
    ˇ;���x�r�ùl��]EƵ���^��8�&/Ɠ�C�~5VjݶR�s�4}(���8���KԹB]��&�pnP�Cl�.E��u��8�3����&W��,��\ZKL��,(�ɒm�ã��pV���v+�&*D�+9�d�������ɳ8m��a��(�h����H7b �q��(�C��w7>��L=
    N+ؠr��$P���5aV�3��t��(O�T���%�&m~��K���
    �D�z�v�ԁ\BZ������
    T@�c>���|����1���4T?�g"d�4Sd�Z	���Zt`�E�ٵ(��K�Nx�&c�����%��}m1G�ģ�7�u,5w��̀�G���ףO�"]+�m��$4wxP����^�Prx+'M�
    >Z��j\��~mqXv���m��S;|h���)��I"��U{lR���kţ���5#�����+S_jCCw©g3f�I�����&5�;N�!I2��C���l�+L�/�&Sb��Y�.�t,�7�~�YH�LEτZ��1���Y���@��r��=8����#H�'�{�7����ߟ�@ ^JEQRSU{/�=�.�U��=���C��ZJ��P'i��i�е��������1�Q�z^y�|ȼ���ZJ�C"&�˘���Đ�������L8u��
    ������a��'!-� ���}I�䕵w�ˇr�$�\��f�8�^�%��#&%�⹄��~-�U�Y�8�X;嗏-��������I�\�ʂ��E�y�=RջEQ��]�v=$֗��
    ���ޤ��}�L��@VNV�Q��S����)�V4&H�b��ü�w������t�mp!�n�ߋ!���+�̠����qAr<W��z�#�㥎�kش����,�*��l՘9�e�X��q��04�h뇉3`��Rv̢$"��;Ⱖ�t6HM���W�f!�a�q��a�&���+�{��1��
    �^���t�թ9��Yn�;�iDԤ�?X�eXQn��*5�q�
    rZ���m�#Ђ_(=T1	D�V���5�ɖ
    shiT[�m_�
    �Kc
    �{
    �JC�~�~�YЪQ�2�*k��Q�KG�̭
    �G���9�wre�Ǥ�9��E�CiH�9P,��U�X�x�C#�1v���I�>\^��.��C7|v"�𚒈+�L���%[�B���v�95�[�PK�&B�Y��2:'rtsp_demo/demo_vdec_vdis_rtsp_bits_rd.c��S���g�+�9F&��iS�=���i^���d��%G�Cy-���=�Iw��MB3�i�}گ�����SZ��;��.y�����m�Mg	��:�ow:dB��b2�$Z�i��w;�ad%�!{d�$��V��榙xM;��$�+���)O^O2�
    }|�V���oY���vw�|t=���C�Cm���浗�f�4m��<����~���t(y	Z��is�J�s�P�J�9-��u1H
    s�q+N��������"�E�r���-�v��ռ��0�L�[���'eu��9�n����+x���UU�gVD�9r�m#;��^@��ޘ�#����<�<>��S��d��?�	(�I���I�48:��y� V4���f�j{��Zm@��SR#���'Q�~B���F��㹹T�x���EaTd��ld��ۥ��iw%�֢$^���Q������"`�+W0wScD.�#0�~�d�<	�N�ơ9�E��ya�_[�~�j�O�������ep��pFbE	�TB��0H�П�EJ�s�y��>h|�(}���%]YWSP�����hi'-�Ѐ�)@�/�0��p���4�s�9u��s�AAO��3��KNh2�6���(�*&�!}������b��7]F�'
    �Q�Ъy�z��fw�?���X��L�c�_�t~�oC�_��>W��[1�������"��_GK7֮�x�<N$~:4&�Av)�Y����r$?�{f��N}��m�W����K�aF��0p�.{��<X
    ����
    �s��;>o�}�E����¾��Z�Lpg��K3���*�s�A���Lx8�����1�G^����gu��W���}jڳ��d�I��K����"'���)ú�N�ATU�a��6�I������N�[�"LJ^��M�����V��Ų$�LR��.K��#�4@z68�ŭ���"��|��&"�0���ۄ��'n"["�~�|Ө��1rv5&q&$y�([�����>k&��	�5�H�
    #��D3�=uH�Q8l����c�@"�C� oB/
    ���$!�ݘ�J��b�}�(Qz�xAm��}�A���f�3.�9���ȚS��a^gfnG�7���`4 b�sݞ��N/���<E����D|>u��`>�`��_��!�E�A|�[�e�	�k9�<T�u�L@]�u���Q�M��?����A����S6��6���C�Yo�R�%��!�s�)M��'��(��V_{P�1˓Z=�0�CBg�>�zkt�uϛ�.]/b�u�b��E�]'-�x\{� ��K⇖v
    lz���ؖr~+�Ռ'����SiF��; }�粤2�4a�x汆�?���Vk���.���
    �P�G�a��J�,����Lyu3x�����ֳ�9e9�B�K׆�UA���f�D�p����f���y	Y}���X���р�u��֟��gϺA�.��$/�yLOy�XRL�):/
    mC�B?�e�,:!�VD�e䛅~S��w�K����,�yVIU��riP��*� �_�E�F��.,̵T���"1А]����a9��⺀$�b�E#��y6v}Q
    �(/���Y�x��I}A����b�N�UC[[U�^�}ZqL�D+��W��]����� c:gy��#7>Rsi�~�p��_N���~���|��o�v|xj���QGmma�U�`
    �p��j�ϵ?�$f�~G�E����\^���\8��TfU@E���N*|�����@�ͱ��U���+{��a+�A��,��Y2w{5��df`W^�:N�e�^���<z���;N�AĨH|�X�_9Q9��P�v�ˢ�")
    ����ְa3A�庤\�z^�1����!X����^����d�?~g
    ����y1B�������i����QE"o�i<���Y���?�٬5L�]�i��������$��-���Q���[X!�mf�����2��'���V����0<����J�C*�B�ӆ�O��
    t�U�Z�����5j�̘N���H%�*���������t���M�W#����u��'F�m��9�
    ��)%��tIa�^���Ʉ`�h
    �B��@3���81���9=�ۜv�3�x���at���08�)c�z(�Pm��1���X�A3�z�`�����xoQ+�'���iڟ*�
    �*C�K���i�*��1Y2���(D�%Wk�x���X1,,)	�����j�٥��Tj�+T�+86آ�������������ȸ�o ���u֪���&�[��4/emQٷ{s�<��=ei�
    R��Z�nF����E����i�-�KM�P�:�4�|3��/E���=���d�"(�L1��Ff86	r*�
    �jͼ��F^r�('���
    �=3'�Ә�߰T��SM��~���V)_
    ���׊�w�.`���f&��$ȧ(��eU~�NA���U��c�{�
    ῊƊ4q�.�  �S�W�A�@ %]�Wg��}�.
    V��1�P;�j���V���~s��f�Ns������n]�Ö����`�7����!���ή����ӏ5�O5�
    "�����շS��WdZ/$JȪo@+\d���=_�y6pc�	�?V�IzuG!EX~��a;�x?h���-.H��-�1�j��f!ܻӋrջ՝-czv�<�P�xI�ʼ�����_�Ώ��	S���8�y�j(�}��M�K��ޖb@�OH`{�L�Xɠ�‚��k"o=�<�jR��0<��?��`�X,���t܋�C���0�!e��:�6zZ=�i.��Đ�(���`/��.Vb�O�p�V��U�yO�7��/�gr�{e�9C������:�'�X��C�dd0�>3!]N)�l� "{��t�
    (�k+�w�4�&��Vw�]�
    �b�4�&3 ��Pb]�KU��N�ݭ��wWȷ�#��{J��4��}�RD��W$\=��B���v�Pĭ�R|�	�wr�)�(#���$V�Jμf�G��_��:_���~�E_{��
    r~E��ώ�'��~������,��ט!E%st>п{hJ���'9`c�4������?S9o/��U�XѷÑ�)KL�X�ס��������� �	D��$ȷ�F�$��[sLk�6���d$k�S�~w��]����s-��s�"*��<�w5,�
    \��p�$�m��z�7�y�Xl�!3���^�sh���Cl��ED+�;�U��5��K�Ϧ+�z�y#�r�a����������k������d��zV�|;�˗��v��9��2���)����f�ɉ$C�ƤW�+��}jE�l������Q��`/�IdO������_E횹+D��$-d�9�l��jV����/����IYe��'�S�'�0���=8&Y��?;w8��_�x��dD�����
    #:`F�v8(?���G��Pn;��M������&��A�i��@�QW���L@g�v_�g%2����G�sv/I��:xΥ��i~�H��{*�2Ht�4��"�	߂��Z
    (���ޱK]O(��ζBVB���H�_�W&�I���q+�[<�	c��*m� �����V�MB�Yz���Պ����
    �,��$�԰"��������"+\�w%l8�	V
    xO1�vA��~o�+��c��PK�&B���E0Vrtsp_demo/Msg_Def.h�<�s���?'�������\>������Z8�
    ^��d�^Q��676x'������%B�d��Roޚ����j�Z��7�����7�]\�ɿ�rf�93«���f��>��o��r�=�f�{,�պ"�����9���*����<#N�8"dtr�c����KR�Ӓ���z�J��"π|��	�{4%-�%��qIZ�yV�e���f�f�.h�UA�f4-��:]��F�qI�(�H���6)MX^��7��7LJ�o���醒i��,�<Z#�H��c�1U�[Z��~�-���|��o��5�z�Q0���w�\�(���U~��L*A��phB^E�b�ٗ���!�V���̿����`�%���%/�cl�<Z����ݢܖ+�$tAJZ܃�[;@/VE�ߑy�L��̫t�V�Ę9�@����)�4KJ4`	u�,���E\��
    ����
    (����
    �l�]PysjEAh�!����=l��vM������	�ǠG0�W��s�Gcߘ�|�z����X�9��S��D����V��f��X�m�:�W��7WNhG��pM���0?L4<>];�o���s�o�j�熾�
    F8꾜���g��
    Ì.�Pӂ����#���}	�`�c�*Xvh�=q|���X7�ky7CVP{� ��4�3q��U42$ص
    ��]Xx;�����N��}��Qm��6C����(�
    ��4�&u]ǽ���Le�)8U��:S{�w&Y����N����=���]��ӛ�k\LTȉ}m���|��d����c�/�#���V{p�(�O�KO���n¡��p���	fCks��~�`� �|�R���?���C��ֵ�Y��#�TYJ85�7����A��?�D;���x��=�y���A��j=%��EK��֟d�xb��cݺ�������Z�:{��,{*�3o2�(A0t� �MN�vE��q1%��Wt['a����'(%ٗ�RTyC(�����z=���\��+s�nO����N.iEB�*���Q��*g��J��ڑ]^T-�ʵé|�Pf��U۸��y�3çE�U	\hd��%w	aa
    m��Z-]#�Ti��
    ��0%Z
    9j��$N��9�§N6���_�`��,�1��>ď
    G�J]a+�c�	l������-��s�gQ�K
    �R�,ުfB��7�o�XvqY>�E�a{K��2���`���B�3��ܕ}
    p�=lb��(;��$�;jga���1"��#�zqW����-��G���2��cA��Ř�W�:&O����%ڟ�{pܬby7t&|	{B�c��@���?c�8c|��k����p&�`X>��-?vZ��AL�o��s����.hz�U��Δ�䦩�����V������_�x0��3T��ӎl+��7�31���
    ���Ze��Fӿ��XT�ee�\��9�a�F�t�sA/�!�n��o����T8�f$2�����f��Fewׂ@�jJ��kjtt��k��k��7�醸�B\7����|c�k��D� ���!��o�N�W��Ƶ` ��J��ְh�ڤ���H+ת���(�0i�(�I�F��+�\#��(|U�kd5Q.�rm�;QN"�G��G�r���q�E9��(�����?]�s�@
    O6j�g鮼 �>H_�:/+���C�F���N���S;b�+ۚw�!�XQ8,k��;�[�D��V0u6B��e%��&r{P�m{�͢n�o@[ہ�f��-�K�H��
    6��".�Y�Zǻ<hEB`���y_���%*�_)}�e�l��`f>�.�����|ي<�0yF��M\�D\;���5hX/_�J��^��{�Ԑg�2/���`�V�{�Ll�"^��:/r#g),����Ծ��7uJ������=#�����*�t�������~XK����f;��(�@�4�gƤΙ`�?��O�ӄ�d���}�c5"�B�$`GQE�hkI ���8[�\yK���H
    ~l{�Գ���U�"ӛ^x�hX����Y� 6�=˃�1D��O���O8�0l1<���<�e��iS�n�#�ܥH�2��FL�:u���9�-`8��}��*�4lK�j��,7DӘT�V{�2ϙڽA�V5�)8�#G��,R|��G�3����6�#P���M�:�N��R�J(���8�"k�Vh�왂���FhQ=�[�V�P?;H�С~z�!M�[F�J�q�P2�DƲCL����Y��Y��[�5�ۙP��0�IԖ�e�8~j���W1��IA7N��lA�^�uf,P�#��iX�;���-J�$���q���gx�J�PU��%L��;1`��v㣆���a7>��S�WAT	5\R�U93���	�?z��P�4	�
    �=g`��U\�Q��ڳou��J����ot�+�7FL�x�^i�#��#��#��#��#��#��#��#��#��#��#��#��g:��t���t?��~���L���N�3��g:��t���t?c�7�����c�.�^(�Gźt}��2��2/�k�w�����Q�}Y��vkΘa���:�~�خ	�H\7X+}�_w��>�Ǜ=ŭF����B����&_|Rk ��.�c�.�c��m�,�͑lK�M�[��K�Ѣ���OF�nNf�sm��;zSl�țaK�7��"�o¤�7� ݱ;wY���ܱ��j����MK[�վ�5���.�D����������674.H��'�JCo�&HWY��=�X.&�b����d�x�i�.'��#�t/����Z�봢w�-�����.V˟ď��Wu�ʁ}�%�� ïa{q��&V�(���l�4��l���#C\6zۃ�增�?B>>�eÄ�d��8e��K�q���n4u��+����8�pczx#�߾ce�7��'�@U���������O��zGJp��
    ��4�q�+��9/�����~K5|��	�}:�Է����>]NJ������<�� ����N���o׶�b�Z�n���0�ԉ.��`�M�g<0���ךw��
    > �_y�;V�B�"�m�{5R�SV�v'��q3�>�0�"�Pa
    �Vy�|OfyQ��1�O��b~[��o�t���r��~�I�I���3P�u#��D��@O-�m�ǺBV��Pj��v���,����+�}���p�r�m�Wk�ù�ēZ��d��+�q	j=*x��{����IP�v��]�͏>��%�T&��i6��:,�(�d|K`ԺD}�T3�=���4����34lg]\*���q��uS\${��෌R��/X]���"d���>���q�C��������,9V�O�6�*U/��!/;H��g��?ƁG�y�7���#_ò��1��x��3�geg�r��L/N��ʹ�-<��ц<>7���=c����s�)����?�y�V�EvQ�mي:�q̏�4�5xc^��0϶��v;�Y�B��g"�����VP=�c����/�E�GG]�E���e`��� xۅ���3���n�˒�O![��U�Fq�)r��U}����ʓ=��`�N���2���%;��?-++8�!�(���D��q��s�2���-S� ��E��k
    �z�i�pb�Er=E�k���/5�<N8
    Yg�lI�? �1΀�? {��������h�e9?R#���1.��!,r��G�I�I`z�.+gG/�-�=b+��dFs��-d9A��w��m\Wk� ����07O�u��NW�M�Xj(��k-��������D-�y�tYNe��5�����3��t�@jG=m���z�nN\#��x�&%i���h`�.���8�z�n[}���� ->x�K�$�z_%���
    =���n��8i/�J�,��~�|�c"�~�;
    �֮����3�LW��li��v�Ǟ�o�%�wO����w1\õ�r��!`T�5�%rv��ح���f��/Y��a�BH`���r�/aݦoK:
    �Ed�"�
    H#������6���ڱ`�ث�(_'l�m*�%y(�����Ũ�[�
    ?�qY9=�M��v�$��u�^F��r����3љB�NG�N!z�#z���#�A!�QG�B���'��g��
    ����'*�~@NU2��OU��j
    �Z�Tk��wG���o�������܋?�5�7n�3[�k���W��xQ�'���M+eU��D�d�Z�mɗK����3�7Q���鿨���&�Z�^S,��7��B����t�o#B�+Q�hV�
    l*=��`+�q���AA�����y~��詵 ��/�v�Z��@n�'�3 �b>�Ad-Ϲ'�/^�%�}	�9%��̅Q����6�I\�~pp�ZOPM,�ppA4JA9�I�0���:�.��x^�+)صݻ�r)�$�
    *4�Wh����fM!����k�����{ ���&��v�Q�u��_,%d�E\�_j�\oӺ�@^��=����4C�%~
    R��p�8�!�x����U�^ݗE\�$S+��9��<^���|���3_�.��:jV�omp�z��������U�k��Qs,1pz}_$�
    H��r�_tM�YB��W'X�8}}Ӹn�-����}z�TG��WMkVc���n�� ;�E����`��)��i{��"��%��e�g�mQ׼���]hqN+�B=�f2���|s�&}�|�Ȏ7�b�7�f�l.�����+���X�.�會|vx�a��[W������,-�*=��x���uS�u^'ڢ�=�j��4�4����	q�爦�d?���cH��H%T?8������� s�l`G�@,�k��r������_��膚كM�(�7�:�ď�����ڣ��~���}�ʊ�}/G�#߱0dH��d����'_NGg��7�z�cؓ/g?,��}�C~������&¡��/�����{.��X����wU4���h�cL�L]��rͭ�%V��6�dm#�,��3�!�F��?��>c!�~���1<���I�9><>&��r����%���F����H�1�;���?���ۑ?ǃ6�}n��f�>��5S������v�ZVy�ځ%���y����`���r��z���r�<��y���n6�9MdDa�A�%�9���X�o{��/�%z�Z�3���������+D�ť���\�e�C|�����3�u��S:�L�p��N��S;e��1�X�`�e�&���̷g~C��Sp�n�̩lw�������S)��6�r��ԃWg��[m�i��m�M�z��0p����Kv�&-{����l�ٖ����?-��/(����^���y�o��_xi��d�l�55c���z����m���{���	�"�=�pس:�����9|B��S�1`1�dE�b+�b}�شo d�@"@�V�BT��.�8��+N�^r?�
    ���Җ��$��s�-;�U���������2���+�V�(���'y12�#�t4<Xϰ�W�9�'@�:��S�ρ�C�����S�����Y�������5�P-y�p��5K�8D6��s����5���[�?��@��(I��H$��	ٍ֥R��O�k8�/���%
    ��C1�b.#w�5�N#�w��'�J:��/�\�u�;�8���l`4�� �5^��.�^+�f�=M��M�OV1,���k@�4��;�2Z{ļ;w0�˚�~��S��-0{�s��k�/�N�+�p%� c�D���QV����O�,MK�;�0]ږҝ�ك��tX1L<}�a�<L����lz�a0|.�����
    �q�v@H\`;l�6�uD������u>�n�	RljS�����ws��n1ӿM\�d�?E�j��p=� h�����j�v��$j��qz���Y:��#� /Wl ���q�1���Z�>'ռ�i�� ��7���M�p�=U�lZ��hR�7��7Z��=iw�	��,}&9�p6�j��4Z��TM�'����V2T}��ְ�����1��dJ����i�-��
    u_8(]�����;�oxt��3*�1����8�F�qJ��}��4����,�Gg"����t7�f��/c���r8��e#�>�(��PK�&B��܋�_rtsp_demo/openRTSP.h�Tmo�H���#�%�(�Tj}:�q�X"�lH��2��u�k��\��~�&���j-!���3�̛���C����Z%j��+JA���E=���D���F�um(0��\������P��*b
    
    ��R���>M0�ZS���*�0�ל�0f)�B���]��{�"C+"~C��ä�2�W��J����S�Gm@Y�������]��=�Ĝ���1�_�1�G���v���;Rm�TV{Ns��Fw�0%��sE~*թ"0ш(d�(0<�d�8�5�ZӼ�m@$|��bN��>�Q�O�K���xK����g��W�0{��� 
    F��o�q8_�<��|2�c2�F��̏�a����l:6�?kD.)%�;�&a\wYb�5*�ɖ���mQW�J�d�p)6M�H8U�����
    ;�p��l����mE�i��B�c�c�`t0d9:r)Un�6~�C���u���v{��'��w��B�i(�)\�W������~��m�r�wB�N����dž6h���t�։��(K�\%%���mzfK�$�±�<����@���>��>�Mr�z
    �ﴤ�4&r�r\�V��`b��ъ\��	zn���J+^k�#���V��N.��M%Gr�D�4r��5^��{��/g�����/��Cx7�Z��[�Q�E�h�'�L��j����~�I����g�|$�=�u}? ��+jS�%�SC�'-�8�2�ZD�/���<D�3�����2u�>Q�3#q�0����w���6A�r��lD�I��`q5�5��mNI����o��z(k�Y�%�Ộ�	�F��0��y�",�j�~2��3�vcMS�A��/E�_^��6*������E�R%�@��V����J�u���C�A~@c��ijV�Bjn�S\�˳k�n��`!&�)^\yGN����y�	8���5�qZ����PK�&B�ʱ�(
    rtsp_demo/rtsp_client.c�Wms�F�\~řL�4��P�q�3Cb/N;MF�	.��H���w�NB�����޳��y���(�-�!�V��u�U�f1?O�̥!�-�=~@{���/�֎��@>O�:�����zp�6=��BjJ�sf��bC�g8!��tE����?��ۅg9����ԫ�2��l?�����Oc0�g�d6�7���Bm�q����4�W��s����.1}ϣ&Y��O�=���:i����x��^�2N��_*�u|��6
    u�����1���n5V��#O����A���࣢��c���M�\v[�w�ί��E����ťv?�hSw�5s��+N�u�2��ߢ�߿mu߿�7I����JE�l?��R���k�c
    ��ح��]_�\We@(zn+��ސ���L2D����G��iE�[���9����y[aO��m��5֔��3�!)��i��]8�o*��U�q�m7:���4©H͖�,�0[Q��z{m.'�6�a�pi�ZIr1S�=���	O��l񢔛�$�fꕍ��Z��@e!��=����IS@&Ԥ[ʶ�"�z�7:,ym�]�!���/3)c�N�oW�����(�j���ɛ�7I��M(�3�w��4N���U���
    Eo�(��|�J�#!���Bz,�	ZH�&�p�>��7g<q*���h���!S}��UY�����Ȗ�Rߒ �0%1J�ɸI�x�Dtf�[&	q 	g��N��Z�{��C�^. �n�{���;���t<�*�T&�(3xRN�x{��2~� �eu���4L3��J�}"��t>��鱡P(p}6���>��%i˴Ɖ�Ti<LM(`W�v=�*���f<Փ�Oя�vb�k��\�����+Uҡ���� U��G�
    T-�Es��[=�}���KK�;�yr���=��{�x����KfM&GӢ��U���bU|a_���;.wK�j�ɀ}BL�Iď3�kڈz�
    h���gj��X�(]6�*
    ?���m�o���/�S0�S
    �9�0৻�������"R��+̧X(|���PK�&Bd����rtsp_demo/rtsp_client.h�T�K�@����~Iá��Q�!h���wG�z�B��4#�ݐ�=������X���yo��Yf�*����<�c�[8*��b��<��_qp�^���U̦.�
    FqJh�qV������B��$�<�)(�9Ѻr]�"��b��^���w��VX��S	$olUg��֔u�C���e�3��]+;��b|=y�l���+~��-���
    ��0��ߣ��G�র1��J��^.U��>��Ն]�Z���d[�xgEw�$|�`/c;#�Ykpo��g�}��ȇK:��y��_��-F!$��^o�U����)y��@��1��8%.U���l�����4�^���ll�TK��g�@�h���"F�k�gg[�o/&�Z�ƶ�<�޸L+劬ţs�N���B����p:/(��o�v^�굁(+���@�K�æ���][��Xx���e�^^�J�ePK�&Bj�����rtsp_demo/share_mem.h�Tmk�0�l����Cb:;��Xi�5���6��ڍ�Q�S,fKF��e��}'�)K�
    y��^����(���w��+frxӎǗ�qo:���M�~`�딾Cz�U��b�h��U�V0ΕQX`j���48�v?��Aq0���V�,�F�ߩ��^��lI0�A]��df�L�d
    \52�4B:�B�()#�k���Q�"i�S$g5�%�MU3��o�xŁ ��M���ΩlRb��6�9@o�Qk0B�^����sH��ao2HF�Q2L�EF!��O���z������38��=�Y7�xCPȹVM7��K<�fY���k���pi/&_��n�:_r�����ꐪ�l�H�U��!�8K��[�B�$���V[پ�٥����m
    ?p�9�(�N��+��.�zu폆J�fZ��P"{&0A��D��́�Y�lSP���|S�:����v���N�w�\p�h7��t	�F����#R2����Z���m7N�}�����(�hv�N�vJ{��B����X�X�Q�*�#�v۸�T�(�Kbg#R&E&�/iod���tc���I��q^������`�U��1U�j==������NɄlw���9�,�ߣO8۞��,��m�S�vV������4Z��CB}/���3}��=�-C�ӑ$mPK�&B��e��
     rtsp_demo/demo_rtsp.cPK�&B,��� �rtsp_demo/demo_rtsp.hPK�&B���
    �< �rtsp_demo/demo_swms.cPK�&B��U�	 rtsp_demo/demo_swms.hPK�&B�Fu
    3 rtsp_demo/demo_vdec_vdis_rtsp.cPK�&B���ԓD J&rtsp_demo/demo_vdec_vdis_rtsp.hPK�&B�Y��2:' -rtsp_demo/demo_vdec_vdis_rtsp_bits_rd.cPK�&B���E0V �;rtsp_demo/Msg_Def.hPK�&B��܋�_ cTrtsp_demo/openRTSP.hPK�&B�ʱ�(
     FXrtsp_demo/rtsp_client.cPK�&Bd���� �\rtsp_demo/rtsp_client.hPK�&Bj����� �^rtsp_demo/share_mem.hPKKoa

  • Hi Badri,

         Thanks for your detailed reply.

         I will try to connect the live555 with decode link according to what you suggested.