Hi,
I'm trying to use VLIB Simulink Blockset (on Matlab 2008a) and export project to CCS v3.3. Unfortunately when I try to create project and build an application i receive followind error:
undefined first referenced
symbol in file
--------- ----------------
_VLIB_extractLumaFromUYUV F:\\Directory\\Video_R_W_ccslink\\CustomMW\\wrap_VLIB_extractLumaFromUYUV.obj
>> error: symbol referencing errors - 'Video_R_W.out' not built
>> Compilation failure
Build Complete,
2 Errors, 4 Warnings, 0 Remarks.
I can succesfully build and run example test project provided with Vlib but I can't create project from Simulink model if it contains Vlib blocks. In addition other models which don't contain Vlib blocks work properly.
Anyone could help me with this?