This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IPNC Reference Design on DM36x Streaming RTSP Into MATLAB/LABVIEW



Hi everyone,

I am working with the TMDSIPCAM8127J3 which has embedded DM8127 video processor for 3D Measurement. We need support in integrating the Camera with Matlab. We have found that through GigE we can able to connect with Matlab. But when we run the following command we faced the below problem. Kindly help us in resolving this issue.

>> obj = videoinput('gige')
Error using videoinput (line 228)
There are no devices installed for the specified ADAPTORNAME. See IMAQHWINFO.

>> imaqhwinfo

ans =

    InstalledAdaptors: {'gentl'  'gige'  'matrox'  'mwdemoimaq'  'winvideo'}
        MATLABVersion: '8.0 (R2012b)'
          ToolboxName: 'Image Acquisition Toolbox'
       ToolboxVersion: '4.4 (R2012b)'