Other Parts Discussed in Thread: TMS320C6748
Hello E2E Community,
I have an OEM hardware that uses the C6748 DSP processor and I am trying to boot from UART2. I have tested using the C6748 LCDK and was successful with the following information displayed in 'Uart Boot Host' program from TI.
(File IO): Read 454072 bytes from file C:\Vantage\TMS320C6748\demos\edge_video_analytics\Release\edge_video_analytics.bin.
(Serial Port): Opening COM26 at 115200 baud...
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 422336-Byte section to address 0xC0000000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 248-Byte section to address 0xC0000000.
(AIS Parse): Processing command 2: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 19700-Byte section to address 0xC0690AA8.
(AIS Parse): Processing command 3: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 96-Byte section to address 0xC06977A0.
(AIS Parse): Processing command 4: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 512-Byte section to address 0xC0697800.
(AIS Parse): Processing command 5: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 396-Byte section to address 0xC0697A00.
(AIS Parse): Processing command 6: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 10688-Byte section to address 0xC0697E10.
(AIS Parse): Processing command 7: 0x58535906.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Performing jump and close...
(AIS Parse): AIS complete. Jump to address 0xC0000000.
(AIS Parse): Waiting for DONE...
(AIS Parse): Boot completed successfully.
(Serial Port): Closing COM26.
When I try to boot on my OEM hardware, this is the error I am getting.
(File IO): Read 454072 bytes from file C:\Vantage\TMS320C6748\demos\edge_video_analytics\Release\edge_video_analytics.bin.
(Serial Port): Opening COM10 at 115200 baud...
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(Serial Port): Read error: The operation has timed out.
(AIS Parse): I/O Error in read!
(AIS Parse): Opcode Sync failed after 11 consecutive I/O failures.
(AIS Parse): Boot aborted.
(Serial Port): Closing COM10.
Can anyone give me some insight as to what the problem is and what I need to do the get it to boot properly?
Thanks,
JumpStart